All about
Explore more
Explore More
Do you need help with your product selection?
Easy setup, low weight and improved operational reliability with SMC’s wireless system
explore
Help & Support
Manuals & downloads
Resources
About us
Our commitments
News & Events
SMC is aware of the recently disclosed PHP vulnerabilities (CVE-2026-109618 and CVE-2026-109619) affecting web-based systems globally.
SMC extends its deepest condolences to those who lost their lives in the 2026 Kumamoto Earthquake that occurred on July 28, 2026.
SMC extends its deepest sympathies to the people of Venezuela and to all those whose lives have been impacted by the devastating earthquakes. Our thoughts are with the individuals, families, and communities facing unimaginable loss, as well as our colleagues and partners in Venezuela during this difficult time.
SMC Corporation (SMC) has received cybersecurity certification in accordance with IEC 62443-4-1:2018 from TÜV SÜD, an internationally recognised third-party certification body headquartered in Munich, Germany.
SMC is pleased to announce that we have received certification from the Science Based Targets (SBT) initiative*¹, an international certification body for climate change, for our “net-zero target” to reduce greenhouse gas (GHG) emissions across our entire value chain, including Scopes 1, 2, and 3*².
Når DIRA Business 2026 løber af stablen, er SMC naturligvis med.
SMC is pleased to announce that we have been selected for the “A List” Company— the highest rating by CDP (Carbon Disclosure Project), an international nonprofit organization that evaluates corporate initiatives on environmental issues, in both the “Climate Change” and “Water Security” categories. On March 17, 2026, Ms. Nozomi Tomobe, Executive Officer of SMC attended the “CDP Awards Japan 2026” held at the United Nations University in Tokyo and delivered a speech.
SMC’s energy-saving initiatives at our factories, aiming to reduce greenhouse gas (GHG) emissions; “Challenging the Limits of Air Reduction: Decarbonization through Air-Saving Equipment × Lowering Facility Air Pressure,” won “The Energy Conservation Center, Japan (ECCJ) Chairman’s Award” in the Best Practice Category of the FY2025 Energy Conservation Grand Prize.
The new flagship R&D hub will accelerate the development of advanced technologies that directly support SMC’s innovation strategy and customer needs across Europe.
SMC launch PFES, an electric speed controller, offering remote control of pneumatic actuator speed with a simple and compact design. It is ideal for installations where access is restricted or puts operators at risk, and it is time saving for applications with multiple speed controllers since the commissioning can be done simultaneously. In case of power loss, PFES retains its last set position ensuring the pneumatic function. Besides pneumatic actuator speed adjustment, PFES is also suitable for the control of air blow or gas purge flow rates.
SMC launches IP66 bar‑type ionizer for washdown and dusty environments Global automation specialist SMC has expanded its static control portfolio with the launch of the IZSW10 Series, a new IP66‑rated bar‑type ionizer designed for reliable performance in dusty, humid and washdown‑intensive environments. The IZSW10 combines high‑speed static neutralisation with long‑range capability, selectable ion generation modes and a hygienic, easy‑to‑maintain design.
SMC launches the HR□C series – a compact and energy-efficient chiller range using CO₂ (R744) as a natural refrigerant. Fully compliant with the latest EU F-Gas Regulation (EU 2024/573), this solution is ideal for manufacturers seeking sustainable thermal control without compromising performance or safety. The HR□C series is designed for easy integration into industrial systems and supports a wide range of applications where precise temperature control is critical.
New from SMC is the PFES Series electric speed controller, offering remote control of pneumatic actuator speed with a simple and compact design. Ideal for installations where access is restricted or puts operators at risk, the PFES Series enables safe, efficient adjustment of actuator speed without the need for manual intervention. Of course, the PFES is not limited to pneumatic actuator speed adjustment and can also be considered for the control of air blow or gas purge flow rates.
For optimal funktionalitet: • Dual-channel ventilkoncept –én enkelt fejl kompromitterer ikke sikkerheden • Certificeret i henhold til ISO 13849-1, op til PLe og SIL 3 i henhold til IEC 61508:2010 – kan installeres som en sikkerhedsrelateret del af styresystemet i overensstemmelse med ovenstående standarder • Høj flowkapacitet – op til 15.000 l/min (ANR) sikrer hurtig afluftning af den farlige energi, som systemtrykket kan udgøre • Soft-start funktion som standard – forhindrer ukontrollerede pneumatiske bevægelser under opstart og reducerer risikoen for maskinskader • Udstyret med port til trykmåler – muliggør visualisering af udgangstryk og/eller integration af yderligere diagnostik med digitale pressostater VPX er modulopbygget for at sikre nem montering sammen med SMC’s luftbehandlingsudstyr og tilsluttes via to M12-stik. Et integreret LED-display giver visuel feedback på ventilens driftsstatus, ud over verifikation gennem styresystemet. “Denne sikkerhedsventil er et velkomment supplement, da den både komplementerer og opgraderer vores sortiment af sikkerhedsprodukter,” siger Fredrik Edholm, Product Manager. “Maskinsikkerhed står øverst på SMC’s dagsorden, og vi leverer effektive produkter til vores kunder, vi bidrager med ekspertise på området, og vi engagerer os i sikkerhedsdrøftelser med vores kunder, hvilket er ekstremt vigtigt,” afslutter han.
SMC lancerer IN778 – en kompakt membrangenerator, der producerer nitrogen fra trykluft uden behov for strømforsyning. Denne løsning er ideel til applikationer, hvor der kræves en kontinuerlig forsyning af nitrogen, for eksempel i fødevare- og medicinalindustrien samt på dækværksteder. Generatoren er kompakt og tilpasset til modulopbygning sammen med SMC’s luftbehandlingsudstyr, hvilket gør den nem at integrere i en maskine eller direkte ved anvendelsesstedet.
Join our Nordic Baltic team in Herning from September 30 to October 2, 2025, where SMC will showcase some of the most exciting and cutting-edge innovations in automation and digitalization. We’ve never launched this many remarkable products in such a short time — and they’re designed to meet the evolving needs of modern industry.
SMC has launched the VPX400 Series Safety Exhaust Valve, designed to provide a quick exhaust of air and ensure superior safety in industrial pneumatic systems. Ideal for emergency stop scenarios, the VPX400 offers quick removal of residual air, mitigating the risks associated with stored pneumatic energy and improving safety for operators.
Smartlift, a leading manufacturer of innovative lifting solutions, has optimized their vacuum technology in collaboration with SMC.
With the new IZS51 series bar-type ionizer from global automation specialist SMC, machine builders and end users can enjoy rapid static charge neutralisation using a compact device with the option of a fully integrated valve unit. The combined ionizer/valve means even more savings in space and wiring, alongside zero flow consumption in standby mode.
Den nye HF2A-LEY er designet til at imødekomme kravene i fødevare og farmaindustrien og passer perfekt ind i maskiner, der regelmæssigt udsættes for desinfektion og rengøring. Cylinderen er designet i rustfrit stål med IP69K kapsling, samt materialer i overensstemmelse med FDA (U.S. Food and Drug Administration) og fødevaregodkendt fedt i henhold til NSF H1. Cylinderen er udstyret med en 230VAC-servomotor og giver præcis positionering i applikationer indenfor fødevarer og farma applikationer.
General industrial equipment designers, manufacturers and maintainers can now benefit from the new SMC ZKJ vacuum manifold with PROFINET, EtherCAT, IO-Link, EtherNet/IP™-enabled communication for remotely controlling and monitoring manufacturing processes. The ZKJ also offers impressive suction flow rate taking its low air consumption and low power consumption specifications into account. Other features include valve protection functionality, IP65 rating and the ability to control up to 16 ejectors with a single manifold.
Global automation specialist SMC is once again extending its innovation credentials by unveiling a clamp-on flow sensor for liquids. Notably, the new PFUW series uses ultrasonics to measure the flow rate of fluids travelling inside piping. Users can deploy the sensors to measure the flow of various liquids, including oil, antifreeze, chemical fluids, water, beverages and more.
To perform in demanding operating environments such as those prevalent in the food industry, SMC is unveiling its advanced HF2A-LEY series rod-type electric actuator. Features such as IP69K-equivalent ingress protection, the use of stainless steel and FDA-compliant construction materials, a smooth profile preventing liquid accumulation and NSF H1 food-grade grease, make the HF2A-LEY electric actuator suitable for food cutting, chopping and filling machines. Indeed, any food processing machines subject to regular cleaning and sanitising regimes are able to benefit.
SMC has been ranked among the “World's Best Employers 2024” by Forbes, a leading U.S. business magazine.
In a move set to help shape the future of Industry 4.0, SMC is launching Smart Assets, a progressive project which will make the asset management requirements of both machine builders and end users fit for the digital age. With collaboration from leading academic and industrial partners, Smart Assets will ultimately lead to the automatic generation of dynamic and data-rich digital representations of all 700,000+ SMC products, helping companies to boost efficiency, interoperability and sustainability. The project will run until 2026.
SMC is unveiling its PSH condensation checker to provide designers and users of pneumatic systems with a highly reliable yet cost-effective way of monitoring temperature and humidity. The new PSH is a very useful device for visualising issues and preventing condensation before it leads to the potential malfunction, failure and costly replacement of important system components.
SMC, a global company operating in more than 80 countries, is taking a significant step to harmonize its international communication by standardizing email addresses worldwide.
New from SMC is the ZGS compact and efficient all-in-one vacuum gripping system. Offering seamless integration with both industrial and collaborative robots, the precise control and integrated design of ZGS series vacuum grippers make for reliable performance in a host of palletising and de-palletising applications.
SMC is introducing its JSY1000/3000-L series 64-station, five-port solenoid valve manifold to support the effective control of more components than ever before from a single manifold. Indeed, SMC is taking the concept of centralised control management a step further by simultaneously releasing the JSY3000-P series, which provides the further potential of connecting electro-pneumatic regulators to the manifold alongside solenoid valves.
Any company building or operating pneumatic systems can now take the opportunity to reduce their carbon footprint by adopting SMC’s innovative new biomass tubing. Manufactured using plant-based biomaterials, TU-TS-T-X309 series tubing drives a reduction in the emissions of CO2 and greenhouse gases. With less use of petroleum-based raw materials, the tubing helps companies achieve a notable step forward in their decarbonisation efforts.
To help dissipate static charge and the often disastrous consequences this phenomenon wreaks on a broad spread of confined-space production machines and systems, SMC is releasing its IZT44/45 series slim bar-type ionizer. The close pitch of the integral emitters make the IZT44/45 series adept at quickly neutralising components carrying a high level of static charge. Notably, SMC’s slim bar-type ionizer can operate effectively without a compressed air supply.
Among numerous major benefits of the new CQE series compact pneumatic cylinder from SMC is energy efficiency. CQE cylinders support a reduction in machine pressure without any negative effects on performance, providing high output force even at low pressure. Users can therefore reduce the supply pressure without increasing actuator bore size, facilitating a significant reduction in energy costs.
SMC Danmark deltager til Foodtech messen i Herning til efteråret. Vi vil gerne invitere dig til at besøge os på stand 7384 i hal J3. Kom og se vores nyeste teknologier og løsninger til din fødevareindustri.
In July 2024, global automation product specialist SMC became a member of the Industrial Digital Twin Association (IDTA). Joining such a powerful community will reap great advantages for the ongoing digital future of the company and its customers. In particular, IDTA membership will ensure SMC always remains abreast of the latest digital twin advances, while simultaneously allowing the company to help shape digital-twin developments in support of Industry 4.0 success.
We hereby would like to announce a remembrance event for our esteemed Honorary Chairman, Yoshiyuki Takada, who passed away on Saturday, April 20, 2024 (JST), at the age of 97.
SMC præsenterer ny kondensationssensor PSH-serien, som overvåger temperatur og fugtighed i pneumatiske systemer. Dette hjælper med at forhindre kondens, der kan føre til fejl og dyre reparationer. Dette produkt er designet til designingeniører, kvalitetsinspektører og vedligeholdelsesteknikere, da den sikrer høj kvalitet af trykluft i applikationer som værktøjsmaskiner, lasermaskiner og fødevareemballageudstyr.
SMC is unveiling an innovative air flow controller that combines a flow sensor and electro-pneumatic regulator in a single product. The result for equipment designers and engineers is a space saving of up to 50%, significantly less piping and cables, and reduced installation time. In addition, the new IN502-44/45/46 allows the precise and reliable control of air flow rate as it is not dependant on piping conditions, pressure differential or temperature. The product benefits any application involving flow control, such as painting, packaging and welding systems across any industry, in particular automotive and food.
SMC is unveiling an innovative elastic finger actuator that boosts the versatility and productivity of automated gripping applications. The rubber sheet fingers of the MH-X7654 adapt to handling objects of different sizes or shapes, thus avoiding the need for specific gripper finger designs for each item.
SMC Corporation is pleased to announce the appointment of Bianca Brunell as the new General Manager for SMC’s Nordic and Baltic countries, effective June 1, 2024. Bianca Brunell brings 27 years of experience in the technology industry, having previously served as Head of Supply Chain at SMC Nordic & Baltic Countries. Her leadership and expertise in the field will be instrumental in driving the region’s continued success and innovation.
SMC Corporation, global leader in industrial automation, introduces an improved version of the ZL1/ZL3/ZL6 series, a renewed multistage ejector range designed to meet the increasing demand for weight reduction in robotics applications, as well as offering IO-Link communication. This product from SMC’s vacuum range offers enhanced suction flow capabilities for workpieces with high levels of leakage while ensuring energy efficiency.
It is with profound sadness that we announce the passing of our esteemed Honorary Chairman, Yoshiyuki Takada. Mr. Takada passed away peacefully on Saturday, April 20, 2024, at the hour of 4:00am, while under medical care.
Today, SMC CORPORATION is pleased to announce that we have signed the United Nations Global Compact Initiative – a voluntary leadership platform for the development, implementation and disclosure of responsible business practices.
We would like to extend our deepest condolences to those who lost their lives in the Earthquakes off the east coast of Taiwan on April 3, 2024, and our heartfelt sympathy to all those affected by the disaster.
During the month of March SMC is highlighting the great women we have in the company. Here you can meet Eeva, Helena and Joan.
SMC received the “Supplier Excellence Awards 2024” from Applied Materials, Inc. (herein after “AMAT”), one of the largest semiconductor and display equipment company.
SMC lancerer nu en innovativ flowregulator designet til at imødekomme alle applikationer som for eksempel maling, emballage og svejsning.
SMC is releasing its LET-X11 series of high-performance belt-driven electric actuators, which provide users with a number of key advantages. Alongside exceptional speed and load capabilities, LET-X11 electric actuators offer lightweight yet robust construction, easy maintenance and advanced auto switch mounting. These versatile products are also suitable for high-speed vertical transfer applications.
SMC Danmark deltager på R24 i år, hvor vi vil vise spændende nyheder frem inden for industriel robotteknologi.
The new SMC CRP series compact compressor allows design engineers to take advantage of an innovative product that allows the use of pneumatic components in areas without air source, making it perfect for use in mobile applications. Moreover, designers have the option of using the versatile CRP series as a compressor (positive pressure) or vacuum pump (negative pressure), simply by connecting the pipes in the corresponding way.
SMC is introducing the new EXW1 Series Compact Wireless System with an increased range of up to 100 m. Similar in technology to the current EX600-W, the EXW1 is smaller, lighter and fieldbus compatible, and with improved features that augment the current portfolio.
SMC provides a large portfolio of products specially designed for secondary battery industry. These 25A-series are compatible with dew points as low as -70°C and include material restrictions for copper and zinc. Explore the benefits of SMC’s 25A products to improve your productivity.
Joan Nowak Høgh overtager ledelsen af det japanskejede datterselskab SMC Danmark, der har fokus på løsninger til industriel automation. Hun skal nu sikre, at SMC Danmark holder vækstkursen og styrker den globale førerpositionen inden for blandt andet pneumatiske og elektriske bevægelsesløsninger.
Do you want to give your robot even more flexibility? Slide into a new dimension with SMC!
At 16:10 on January 1, 2024 (JST), a huge earthquake with a magnitude of 7.6 struck the Noto region, northern part of Ishikawa Prefecture Japan.
SMC is once again demonstrating its innovation prowess with the company’s new JSY1000-E valve manifold with fully integrated ejector system. This optimal combination provides a complete solution for positive and negative (vacuum) pressure that allows users to control valves and ejectors in a single, simple manifold. Reducing both physical dimensions and weight, the JSY1000-E also has an energy function available that decreases energy consumption substantially and improves process efficiency.
SMC is introducing its innovative JSXF-P series of pulse valves for the effective and efficient dislodging of foreign matter during cleaning procedures. The new JSXF-P SMARTVENT type pulse valve offers a number of notable benefits, including a built-in control board, high peak pressure, low air consumption and long service life.
Vi ønsker alle en glædelig jul og giver et kort tilbageblik på året 2023. Tak for et godt samarbejde til vores kunder og samarbejdspartnere, vi glæder os til et nyt år med spændende nyheder og muligheder. Vi holder åbent imellem jul og nytår fra d. 27. - 29. december.
SMC Danmark er stolte af at lancere den nye og forbedrede kompaktcylinder MGPK, som giver maskinbyggere en bæredygtig løsning med markedets laveste vægt blandt tilsvarende produkter. Denne opgradering giver mulighed for let og simpelt design til mindre maskiner, samtidig med at den bibeholder den samme imponerende belastningskapacitet som den tidligere MGPM-model.
SMC is unveiling an innovative air flow controller that combines a flow sensor and electro-pneumatic regulator in a single product. The result for equipment designers and engineers is a space saving of up to 50%, significantly less piping and cables, and reduced installation time. In addition, the new IN502-44/45 allows the precise and reliable control of air flow rate as it is not dependant on piping conditions, pressure differential or temperature. The product benefits any application involving flow control, such as painting, packaging and welding systems across any industry, in particular automotive and food.
The new JSY3000-S is a bottom-ported manifold with stainless steel plate and FDA-compliant fittings that delivers extended operating life in food and beverage manufacturing environments. Part of SMC’s extensive directional control valve family, the new plug-in JSY3000-S is cabinet-mounted with a robust bottom seal and the piping connections facing outwards. This design configuration helps to protect the valve against both corrosion and splashes from water, ensuring its suitability for location near any type of equipment that requires wash-down procedures.
SMC præsenterer en innovativ løsning med deres nye elektriske lineære kugleføring og cylinder, der kombinerer integreret kontroller og nem programmering. Denne nyhed åbner op for en lang række anvendelsesmuligheder takket være den dedikerede software, der følger med enheden. Med indbygget kontroller og muligheden for at vælge mellem tre forskellige positioner er denne elektriske aktuator en kompakt og brugervenlig løsning.
We would like to extend our deepest condolences to those who lost their lives in the terrible Earthquakes occurred in the Kingdom of Morocco on September 8, 2023, and our heartfelt sympathy to all those affected by the disaster.
The new EQ series of slide-type and rod-type electric actuators from SMC feature a fully integrated controller, providing a simpler to set-up, easier-to-use, space-saving solution that simultaneously helps users to save energy and reduce CO2 emissions. As a further advantage, EQ series electric actuators offer straightforward control with simple and exclusive software which helps users to start the actuators working via a single screen in just three steps. First, users choose ‘set operation mode’, before specifying the stopping positions and finally defining the speed, acceleration and deceleration values. It is no more complex than controlling a two- or three-position solenoid valve.
The new JSB series angle seat valve from SMC offers a number of key advantages to OEMs and end users alike, combining long service life, low pressure loss and compact dimensions with a high flow rate. Suitable for use with steam, water and air, optimisation of the JSB’s body flow profile ensures this space-saving valve can deliver the same flow rate as larger counterparts and, in turn, support system energy savings.
SMC Danmark runder i år en vigtig milepæl og har siden 1998 solgt pneumatiske og elektriske bevægelsesløsninger til maskinbyggere og industrivirksomheder. Der er en god grund til at kippe med flaget i Horsens, for det japanske datterselskab har aldrig haft et stærkere produktsortiment end netop nu.
The specialist for pneumatic and electric automation SMC got the "Bosch Global Supplier Award" in the category "Indirect Purchasing and Services" for its top performance as a supplier.
For at understøtte de korte leveringstider tilbyder SMC både globale og lokale lagerbeholdninger.
All sectors across general manufacturing and automation can take advantage of the SMC ZHV air amplifier, a new product that offers high flow rates which are fully adjustable to suit specific customer requirements. This energy-efficient, compact and lightweight solution functions as either a blow-off or vacuum unit.
We are pleased to inform that SMC will be relocating and expanding its current Tsukuba Technical Center (JTC), and open “Kashiwanoha Campus New Technical Center (provisional name)” in the "Kashiwanoha Smart City" in the fall of 2025.
Vi er glade for at kunne informere, at SMC vil flytte og udvide sin nuværende Tsukuba Technical Center (JTC), og åben "Kashiwanoha Campus New Technical Center (foreløbig name)" i "Kashiwanoha Smart City" i efteråret 2025.
Coherent Corporation, a global leader in materials, networking, and lasers, has recognized SMC Corporation of America with the Outstanding Innovation & Technology Supplier 2023 award for their outstanding performance in 2022.
Nu lancerer SMC Air Management System, en smart enhed, der overvåger maskinens drift og sænker eller slukker trykket i produktionspausen. Op til 62% af trykluftforbruget kan reduceres, samtidig med at ydeevnen opretholdes, og brugeren modtager alle relevante driftsdata via fieldbusprotokol eller OPC UA, hvilket giver et godt grundlag for tilstandsbaseret vedligeholdelse.
News from SMC Corporation. As a comprehensive manufacturer of automation equipment, SMC aims to fulfil its product supply responsibilities and maintain the trust of customers by contributing to sustainable growth and the expansion of reliable technological innovations. To help deliver these objectives, SMC has a rock-solid Business Continuity Plan (BCP) that the company is now further strengthening to provide an even more robust automation and motion control offer for its global customer base.
As a comprehensive manufacturer of automation equipment, SMC aims to fulfil its product supply responsibilities and maintain the trust of customers by contributing to sustainable growth and the expansion of reliable technological innovations. To help deliver these objectives, SMC has a rock-solid Business Continuity Plan (BCP) that the company is now further strengthening to provide an even more robust automation and motion control offer for its global customer base.
Vi vil gerne udtrykke vores dybeste medfølelse til alle dem, der er berørt af de forfærdelige jordskælv, der fandt sted i det sydøstlige Tyrkiet den 6. februar 2023.
We would like to extend our heartfelt sympathies to all those affected by the terrible Earthquakes occurred in southeastern Turkey on February 6, 2023. And we sincerely hope that the relief efforts will progress rapidly.
SMC lancerer en ny kontroller med STO-funktion (Safe Torque Off) og SS1-t (Safe stop) til stepmotorer, for implementering i henhold til gældende ISO / IEC-standarder. Kan kombineres med batteriløse absolut encodere for kortere cyklustider og lettere genstart efter nødstop.
Leading industrial automation and IIoT specialist SMC is addressing the need to reduce CO2 emissions and cut energy consumption with the release of its latest innovation, the AMS20/30/40/60 Series compressed air management system. By adopting this revolutionary new air management unit, any company that deploys pneumatic processes can gain from reductions of up to 62% in compressed air consumption, benefiting both the environment and bottom line profitability.
SMC Corporation, a global leader in manufacturing comprehensive automation control equipment has been recognized by Forbes magazine as a World’s Best Employers 2022.
SMC, a leading Japan-headquartered global specialist in pneumatic and other automated control solutions, is set to join the Nikkei 225 (or Nikkei Stock Average), the premier and most-often quoted index of Japanese stocks. The Nikkei 225 comprises of 225 stocks selected from Japan’s top-performing and most liquid blue-chip companies. SMC will commence its listing on 3 October 2022.
SMC’s ISE7# pressure switch has been updated adding higher pressure ranges apart from offering improved flexibility and higher control of applications, leading to better decision making.
The new JSY & ZK2-A valve and ejector combination manifold from SMC not only simplifies pneumatic systems in applications requiring both positive and negative pressure (vacuum), it also reduces wiring requirements, provides complete compatibility with multiple fieldbus communication protocols and eliminates pressure fluctuations.
Any machine builder looking to simplify and reduce the cost of adding higher levels of safety, while simultaneously seeking faster and broader communication capabilities should consider the new JXCLF step motor controller from SMC. The JXCLF features an IO-Link communication interface and a Safe Torque Off (STO) function, thus presenting machine builders with the opportunity to deliver better control of the manufacturing process and increase their system’s safety integrity level (SIL 3) and performance level (PL e) in a cost-effective way.
Leading industrial control and automation solutions specialist, SMC, is adding a new range of pinch valves to its expansive offer for medical device and food system OEMs. With the new LPV series valve, fluid does not come into contact with any moving parts, avoiding the potential for contamination. Moreover, by simply discarding the tube after use, there is no longer any need for a washing process, ensuring good hygiene. SMC’s energy-saving LPV pinch valve is suitable for controlling a wide range of analytical, medical and food industry fluids.
General industrial equipment designers, manufacturers and maintainers can now benefit from the new SMC ZKJ vacuum manifold with PROFINET-enabled communication for remotely controlling and monitoring manufacturing processes. The ZKJ also offers impressive suction flow rate taking its low air consumption and low power consumption specifications into account. Other features include valve protection functionality, IP65 rating and the ability to control up to 16 ejectors with a single manifold.
The new JSY5000-H valve manifold from SMC is purpose-designed for use in food and beverage manufacturing plants, as well as breweries. Featuring a clean design to cope with regular wash-downs, the IP69K-compliant valve differentiates itself in the marketplace with its high flow rate, low power consumption and IO-Link point-to-point communication capability, bringing a new level of control to production.
One of the latest digital flow switches to join the SMC family, PF3A#H, monitors the consumption of the main line with a 100:1 ratio. It is IO-Link compatible, and it offers the possibility of being connected to air combination units in a simple way. And now, an even more complete solution can be obtained, thanks to the integrated pressure and temperature sensors.
A new polypropylene type pump from SMC has been designed to withstand the harshest manufacturing processes, delivering production reliability that lead to cost and energy savings.
The new HRR rack-mounted thermo-chiller from SMC has been designed for installers where space is an issue. It also delivers efficiencies in terms of installation and maintenance, as it can be adjusted and maintained while installed in a rack.
Cobots and end effectors team up for affordable flexible solutions. While robotics led the way for the rapid growth of automation, we see cobots as the democratisation of robotics technology. They eliminate the cost and complex programming that robots usually require while providing much greater flexibility. By Andrea Trifone, Cobot project leader, SMC Italy
SMC has designed a new lightweight, handysized ionizing gun that can neutralise static, rapidly and effectively, from a variety of products at different phases of production.
SMC has designed a direct operated 2-port solenoid valve that can withstand the harshest of environments whilst saving energy.
SMC has unveiled the IZT ionizer series that offers customers a compact solution, with a separate controller to optimise space. The new design also offers enhanced monitoring capabilities, the bars and nozzles are simple to adjust, even when located in hard to reach spaces.
The new Impact Blow Gun (IBG) from SMC is the most energy efficient on the market, using up to 87% less air than any other standard blowing gun.
The latest digital flow switch to join the SMC family, PF3A7#H, monitors the consumption of the main line with a 100:1 ratio. And now, further benefits come together with IO-Link.
SMC has given its popular all-in-one vacuum unit ejector and pump system a refresh with the launch of the ZK2-A series. The latest incarnation offers customers superb efficiencies in terms of space, energy, maintenance and noise.
For installations that require precise and efficient control in challenging operating conditions, SMC launches its new IN-777 air servo cylinder for multipoint positioning and control
SMC has renewed its multistage ejector range with the, ZL1/ZL3/ZL6 series, in response to weight reduction demand that comes from the growing use of robotics. This addition to SMC’s vacuum range meets the suction flow requirements for workpieces with high levels of leakage, while also delivering energy efficiencies.
SMC has added to its gripper range with the launch of the MHM, which uses a magnet to handle workpieces. Ideal for workpieces with uneven surfaces or featuring holes, the MHM provides machine operators with reliable and safe handling and reduced cycle times that increases productivity.
The monitoring of multiple lines within a plant has become easier thanks to SMC’s new PSE200A 3-screen display, multi-channel digital sensor monitor.
SMC is meeting the challenge of speed and precision presented by the increasing use of robotic arms on production lines with its new JMHZ2 compact type parallel style air gripper.
A new digital flow switch manifold from SMC simplifies the flow and temperature control of production lines and facilities by housing switches in a single manifold.
In response to working closely with its customers and identifying a need for space optimised and cost efficient solutions, SMC launches its JSY 5-port Solenoid Valve with the shortest valve width in the world at 6.4mm.
SMC extends its cylinder range with the launch of its new ISO locking cylinder, CP96N-C96N that has a stronger holding force and is ideal for intermediate stops and drop prevention.
SMC at Compamed 2019
SMC’s latest digital gap checker, ISA3-L, features IO-Link compatability, offering manufacturers greater control of applications and more information at a glance with its 3-screen data display.
SMC has responded to market demand for smaller components with the JAS compact speed controller. Its launch means SMC now offers a complete range of ‘compact’ solutions that also includes cylinders and small integrated auto switches.
SMC at EMO Hanover 2019
SMC Corporation announces its fifth year of consecutive sales growth for its European business, posting a 6.3% increase to deliver annual net sales of €745.87 million.
SMC at LASER World of PHOTONICS 2019
SMC has added to its extensive valve range with the JSXFA, a high peak pressure pulse valve, that is also fast to respond and uses low air consumption, to guarantee energy savings.
Japanese automation firm, SMC, has been listed in the FORBES Global 2000 as one of the world’s largest public companies.