Po nekaj letih Industrije 4.0, tovarne prihodnosti, pametne tovarne in digitalizacije smo se naučili, da je dodana vrednost, ki jo lahko nudimo našim strankam, pomoč pri iskanju najboljših ekosistemov rešitev, ki ustrezajo vašim strojem v IIoT.
SMC na področju industrijskega komuniciranja deluje na dva načina: naše stranke podpiramo s posebnimi rešitvami in ponujamo najsodobnejše izdelke. Z našim edinstvenim brezžičnim sistemom in široko paleto IO-Link rešitev opremimo vašo tovarno z inteligentno digitalizacijo in avtomatizacijo.
V današnji proizvodnji stroji in naprave komunicirajo med seboj in jih je mogoče upravljati na daljavo, saj so povezani s pomočjo senzorjev in komunikacijskih tehnologij. Ti so, na primer, bistveni za industrijsko vzdrževanje vsakega proizvodnega procesa.
Zato v SMC razvijamo pametno proizvodnjo. Z uporabo industrijskih komunikacijskih rešitev se lahko posebej posvetimo vašim potrebam in tako izboljšamo učinkovitost in produktivnost vaših procesov. To nam omogoča, da prilagodimo svoje rešitve najboljši vrednosti za stranke, hkrati pa zagotavljamo globalno razpoložljivost in dobavo, tako da vaša proizvodnja vedno deluj učinkovito.
Wireless is priceless in any industry or application that makes regular use of motion applications with communication cables. Among these, one area where this is particularly valuable is in parts assembly, whether it be in automotive, electronics production or any industry where rotary tables and robotic systems are commonly used. SMC’s wireless unit allows you to achieve consistent, noise-free communication with fewer cables, reduced maintenance, as well as less breakage and disconnection on the factory floor.
With robots and cobots, SMC’s solutions are all based on two things. Firstly, optimising the size of a robot according to its payload and, secondly, speed and flexibility. We are always looking for ways to make robots lighter, smaller, more efficient and able to communicate smartly. We develop all our products based on feedback - our customer's actual requirements, based on the challenges they are facing to meet current and future requirements.
Electric actuators are, by definition, a flexible solution, at least in terms of speed, force or positioning. It is precisely such adaptability which is behind SMC’s range of electric solutions; where you decide, you choose, but you don’t adapt to them. They adapt to you. Our extensive variety of mechanics and controllers, and their great adaptability, allow us to say, without a doubt, that with them, you can perform any movement, anywhere, in any way you want.
SMC’s IO-Link products can help you improve your productivity and reduce your costs, ensuring dynamic production processes and leading to the smart factory the industry is seeking. Moreover, they will allow you to guarantee the continuous improvement of your company’s industrial maintenance strategy.
The use of Fieldbus in manufacturing processes has substantially improved the way we handle communications, providing us with considerable savings in terms of wiring, connectors, installation and setup time, electronic diagrams or documentation. For the development of our Serial Interface range, we have gone a step further and increased the number of possibilities in industrial communication, bearing in mind the flexibility and versatility that our customers demand.