Predstavljamo
Potrebujete pomoč pri izbiri izdelkov?
Splošne informacije o izdelkih
SMC e-Matters
Top konfiguratorji & orodja
Standardi & navodila
Orodja in datoteke programske opreme
Knjižnice
Kontakti
Priročniki in prenosi
Dokumenti
Podpora
Dobrodošli v SMC
General industrial equipment designers, manufacturers and maintainers can now benefit from the new SMC ZKJ vacuum manifold with PROFINET, EtherCAT, IO-Link, EtherNet/IP™-enabled communication for remotely controlling and monitoring manufacturing processes. The ZKJ also offers impressive suction flow rate taking its low air consumption and low power consumption specifications into account. Other features include valve protection functionality, IP65 rating and the ability to control up to 16 ejectors with a single manifold.
Global automation specialist SMC is once again extending its innovation credentials by unveiling a clamp-on flow sensor for liquids. Notably, the new PFUW series uses ultrasonics to measure the flow rate of fluids travelling inside piping. Users can deploy the sensors to measure the flow of various liquids, including oil, antifreeze, chemical fluids, water, beverages and more.
To perform in demanding operating environments such as those prevalent in the food industry, SMC is unveiling its advanced HF2A-LEY series rod-type electric actuator. Features such as IP69K-equivalent ingress protection, the use of stainless steel and FDA-compliant construction materials, a smooth profile preventing liquid accumulation and NSF H1 food-grade grease, make the HF2A-LEY electric actuator suitable for food cutting, chopping and filling machines. Indeed, any food processing machines subject to regular cleaning and sanitising regimes are able to benefit.
SMC is unveiling its PSH condensation checker to provide designers and users of pneumatic systems with a highly reliable yet cost-effective way of monitoring temperature and humidity. The new PSH is a very useful device for visualising issues and preventing condensation before it leads to the potential malfunction, failure and costly replacement of important system components.
New from SMC is the ZGS compact and efficient all-in-one vacuum gripping system. Offering seamless integration with both industrial and collaborative robots, the precise control and integrated design of ZGS series vacuum grippers make for reliable performance in a host of palletising and de-palletising applications.
SMC is introducing its JSY3000-L series 64-station, five-port solenoid valve manifold to support the effective control of more components than ever before from a single manifold. Indeed, SMC is taking the concept of centralised control management a step further by simultaneously releasing the JSY3000-P series, which provides the further potential of connecting electro-pneumatic regulators to the manifold alongside solenoid valves.
To help dissipate static charge and the often disastrous consequences this phenomenon wreaks on a broad spread of confined-space production machines and systems, SMC is releasing its IZT44/45 series slim bar-type ionizer. The close pitch of the integral emitters make the IZT44/45 series adept at quickly neutralising components carrying a high level of static charge. Notably, SMC’s slim bar-type ionizer can operate effectively without a compressed air supply.
Among numerous major benefits of the new CQE series compact pneumatic cylinder from SMC is energy efficiency. CQE cylinders support a reduction in machine pressure without any negative effects on performance, providing high output force even at low pressure. Users can therefore reduce the supply pressure without increasing actuator bore size, facilitating a significant reduction in energy costs.
Any company building or operating pneumatic systems can now take the opportunity to reduce their carbon footprint by adopting SMC’s innovative new biomass tubing. Manufactured using plant-based biomaterials, TU-TS-T-X309 series tubing drives a reduction in the emissions of CO2 and greenhouse gases. With less use of petroleum-based raw materials, the tubing helps companies achieve a notable step forward in their decarbonisation efforts.
We hereby would like to announce a remembrance event for our esteemed Honorary Chairman, Yoshiyuki Takada, who passed away on Saturday, April 20, 2024 (JST), at the age of 97.
In July 2024, global automation product specialist SMC became a member of the Industrial Digital Twin Association (IDTA). Joining such a powerful community will reap great advantages for the ongoing digital future of the company and its customers. In particular, IDTA membership will ensure SMC always remains abreast of the latest digital twin advances, while simultaneously allowing the company to help shape digital-twin developments in support of Industry 4.0 success.
SMC is unveiling an innovative air flow controller that combines a flow sensor and electro-pneumatic regulator in a single product. The result for equipment designers and engineers is a space saving of up to 50%, significantly less piping and cables, and reduced installation time. In addition, the new IN502-44/45/46 allows the precise and reliable control of air flow rate as it is not dependant on piping conditions, pressure differential or temperature. The product benefits any application involving flow control, such as painting, packaging and welding systems across any industry, in particular automotive and food.
SMC is unveiling an innovative elastic finger actuator that boosts the versatility and productivity of automated gripping applications. The rubber sheet fingers of the MH-X7654 adapt to handling objects of different sizes or shapes, thus avoiding the need for specific gripper finger designs for each item.
SMC Corporation, global leader in industrial automation, introduces an improved version of the ZL1/ZL3/ZL6 series, a renewed multistage ejector range designed to meet the increasing demand for weight reduction in robotics applications, as well as offering IO-Link communication. This product from SMC’s vacuum range offers enhanced suction flow capabilities for workpieces with high levels of leakage while ensuring energy efficiency.
It is with profound sadness that we announce the passing of our esteemed Honorary Chairman, Yoshiyuki Takada. Mr. Takada passed away peacefully on Saturday, April 20, 2024, at the hour of 4:00am, while under medical care.
Today, SMC CORPORATION is pleased to announce that we have signed the United Nations Global Compact Initiative – a voluntary leadership platform for the development, implementation and disclosure of responsible business practices.
We would like to extend our deepest condolences to those who lost their lives in the Earthquakes off the east coast of Taiwan on April 3, 2024, and our heartfelt sympathy to all those affected by the disaster.
SMC received the “Supplier Excellence Awards 2024” from Applied Materials, Inc. (herein after “AMAT”), one of the largest semiconductor and display equipment company.
SMC is releasing its LET-X11 series of high-performance belt-driven electric actuators, which provide users with a number of key advantages. Alongside exceptional speed and load capabilities, LET-X11 electric actuators offer lightweight yet robust construction, easy maintenance and advanced auto switch mounting. These versatile products are also suitable for high-speed vertical transfer applications.
SMC is introducing the new EXW1 Series Compact Wireless System with an increased range of up to 100 m. Similar in technology to the current EX600-W, the EXW1 is smaller, lighter and fieldbus compatible, and with improved features that augment the current portfolio.
The new SMC CRP series compact compressor allows design engineers to take advantage of an innovative product that allows the use of pneumatic components in areas without air source, making it perfect for use in mobile applications. Moreover, designers have the option of using the versatile CRP series as a compressor (positive pressure) or vacuum pump (negative pressure), simply by connecting the pipes in the corresponding way.
At 16:10 on January 1, 2024 (JST), a huge earthquake with a magnitude of 7.6 struck the Noto region, northern part of Ishikawa Prefecture Japan.
SMC is introducing its innovative JSXF-P series of pulse valves for the effective and efficient dislodging of foreign matter during cleaning procedures. The new JSXF-P SMARTVENT type pulse valve offers a number of notable benefits, including a built-in control board, high peak pressure, low air consumption and long service life.
SMC is once again demonstrating its innovation prowess with the company’s new JSY1000-E valve manifold with fully integrated ejector system. This optimal combination provides a complete solution for positive and negative (vacuum) pressure that allows users to control valves and ejectors in a single, simple manifold. Reducing both physical dimensions and weight, the JSY1000-E also has an energy function available that decreases energy consumption substantially and improves process efficiency.
The new JSY3000-S is a bottom-ported manifold with stainless steel plate and FDA-compliant fittings that delivers extended operating life in food and beverage manufacturing environments. Part of SMC’s extensive directional control valve family, the new plug-in JSY3000-S is cabinet-mounted with a robust bottom seal and the piping connections facing outwards. This design configuration helps to protect the valve against both corrosion and splashes from water, ensuring its suitability for location near any type of equipment that requires wash-down procedures.
SMC is unveiling an innovative air flow controller that combines a flow sensor and electro-pneumatic regulator in a single product. The result for equipment designers and engineers is a space saving of up to 50%, significantly less piping and cables, and reduced installation time. In addition, the new IN502-44/45 allows the precise and reliable control of air flow rate as it is not dependant on piping conditions, pressure differential or temperature. The product benefits any application involving flow control, such as painting, packaging and welding systems across any industry, in particular automotive and food.
We would like to extend our deepest condolences to those who lost their lives in the terrible Earthquakes occurred in the Kingdom of Morocco on September 8, 2023, and our heartfelt sympathy to all those affected by the disaster.
The new JSB series angle seat valve from SMC offers a number of key advantages to OEMs and end users alike, combining long service life, low pressure loss and compact dimensions with a high flow rate. Suitable for use with steam, water and air, optimisation of the JSB’s body flow profile ensures this space-saving valve can deliver the same flow rate as larger counterparts and, in turn, support system energy savings.
The new EQ series of slide-type and rod-type electric actuators from SMC feature a fully integrated controller, providing a simpler to set-up, easier-to-use, space-saving solution that simultaneously helps users to save energy and reduce CO2 emissions. As a further advantage, EQ series electric actuators offer straightforward control with simple and exclusive software which helps users to start the actuators working via a single screen in just three steps. First, users choose ‘set operation mode’, before specifying the stopping positions and finally defining the speed, acceleration and deceleration values. It is no more complex than controlling a two- or three-position solenoid valve.
The specialist for pneumatic and electric automation SMC got the "Bosch Global Supplier Award" in the category "Indirect Purchasing and Services" for its top performance as a supplier.
A new polypropylene type pump from SMC has been designed to withstand the harshest manufacturing processes, delivering production reliability that lead to cost and energy savings.
I’m Yoshiki Takada. As of April 1st, 2021, I was appointed as the new president of SMC. Since our founding in 1959, SMC has grown as a comprehensive manufacturer of automatic control equipment, including pneumatic equipment, with the goal of “meeting all of our customer requests”.
The new HRR rack-mounted thermo-chiller from SMC has been designed for installers where space is an issue. It also delivers efficiencies in terms of installation and maintenance, as it can be adjusted and maintained while installed in a rack.
SMC has designed a new lightweight, handysized ionizing gun that can neutralise static, rapidly and effectively, from a variety of products at different phases of production.
SMC has designed a direct operated 2-port solenoid valve that can withstand the harshest of environments whilst saving energy.
SMC has unveiled the IZT ionizer series that offers customers a compact solution, with a separate controller to optimise space. The new design also offers enhanced monitoring capabilities, the bars and nozzles are simple to adjust, even when located in hard to reach spaces.
The new Impact Blow Gun (IBG) from SMC is the most energy efficient on the market, using up to 87% less air than any other standard blowing gun.
The latest digital flow switch to join the SMC family, PF3A7#H, monitors the consumption of the main line with a 100:1 ratio. And now, further benefits come together with IO-Link.
For installations that require precise and efficient control in challenging operating conditions, SMC launches its new IN-777 air servo cylinder for multipoint positioning and control
SMC has given its popular all-in-one vacuum unit ejector and pump system a refresh with the launch of the ZK2-A series. The latest incarnation offers customers superb efficiencies in terms of space, energy, maintenance and noise.
SMC has renewed its multistage ejector range with the, ZL1/ZL3/ZL6 series, in response to weight reduction demand that comes from the growing use of robotics. This addition to SMC’s vacuum range meets the suction flow requirements for workpieces with high levels of leakage, while also delivering energy efficiencies.
SMC has added to its gripper range with the launch of the MHM, which uses a magnet to handle workpieces. Ideal for workpieces with uneven surfaces or featuring holes, the MHM provides machine operators with reliable and safe handling and reduced cycle times that increases productivity.
The monitoring of multiple lines within a plant has become easier thanks to SMC’s new PSE200A 3-screen display, multi-channel digital sensor monitor.
SMC is meeting the challenge of speed and precision presented by the increasing use of robotic arms on production lines with its new JMHZ2 compact type parallel style air gripper.
A new digital flow switch manifold from SMC simplifies the flow and temperature control of production lines and facilities by housing switches in a single manifold.
In response to working closely with its customers and identifying a need for space optimised and cost efficient solutions, SMC launches its JSY 5-port Solenoid Valve with the shortest valve width in the world at 6.4mm.
SMC extends its cylinder range with the launch of its new ISO locking cylinder, CP96N-C96N that has a stronger holding force and is ideal for intermediate stops and drop prevention.
SMC at Compamed 2019
SMC has responded to market demand for smaller components with the JAS compact speed controller. Its launch means SMC now offers a complete range of ‘compact’ solutions that also includes cylinders and small integrated auto switches.
SMC’s latest digital gap checker, ISA3-L, features IO-Link compatability, offering manufacturers greater control of applications and more information at a glance with its 3-screen data display.
SMC at EMO Hanover 2019
SMC Corporation announces its fifth year of consecutive sales growth for its European business, posting a 6.3% increase to deliver annual net sales of €745.87 million.
SMC at LASER World of PHOTONICS 2019
Yoshiyuki Takada Chairman SMC Corporation
SMC has added to its extensive valve range with the JSXFA, a high peak pressure pulse valve, that is also fast to respond and uses low air consumption, to guarantee energy savings.
TIRE TECHNOLOGY EXPO 2019 5 – 7 March 2019 Deutsche Messe Exhibition Centre, Hanover Hall 21, Booth 9064
COMPAMED 2018 12 -15 November 2018 Düsseldorf Trade Fair, Düsseldorf, Germany Hall 8B, Stand H04 Visitors to this year’s COMPAMED will have a chance to view SMC’s diverse range of specialist solutions for the Life Sciences industry.
A bit of introduction
SMC is building on the success of its ZSE20(F)/ISE20 pressure switch range that features 3-screen display, 3-step setting mode and selectable delay time function, with the ZSE20(F)#/ISE20# (A, B and C). The extended series will help operators deliver efficiencies in terms of control and time saving. Now including IO-Link connection.
SMC's ISE7# pressure switch has been updated offering improved flexibility and higher control of applications, leading to better decision making.
SMC has launched a wireless fieldbus unit, EX600-W, that offers customers a decentralised solution that is EtherNet/IP™ compatible and can withstand electric noise, deeming it reliable even in harsh, industrial environments.
SMC has unveiled the IZT ionizer series that offers customers a compact solution, with a separate controller to optimise space. The new design also offers enhanced monitoring capabilities and the bars are simple to adjust, even when located in hard to reach spaces.
The latest vacuum pad from SMC is the ZP3P, which has been designed to offer optimum absorbing performance and efficient handling. It features a blue coloured, silicone rubber pad that prevents wrinkles and is compliant with the FDA 21CFR§177.2600 elution test.
Japanese automation firm, SMC, has been listed in the FORBES Global 2000 as one of the world’s largest public companies.
The MACM is a new centring unit from SMC that helps to align and position heavy workpieces on the move, so manufacturers can install and operate more compact conveyor lines.
SMC is building on the success of its ZSE20(F)/ISE20 pressure switch range that features 3-screen display, 3-step setting mode and selectable delay time function, with the ZSE20(F)#/ISE20# (A, B and C). The extended series will help operators deliver efficiencies in terms of control and time saving.
SMC has extended its multi-axes control step motor controller range, with the launch of the JXC92. This new unit can control up to three electric actuators simultaneously, creating a range of savings and simplifying the process in terms of equipment, wiring, space and programming.
TIRE TECHNOLOGY EXPO 2018 20 - 22 February 2018 Hannover Hall 21, Booth 7045
The MWB Series cylinder from SMC, features a separate lock unit that has been designed with the operator in mind. Versatility and simplicity are key to this latest design with installation and maintenance time kept to a minimum.
Static electricity is an invisible but costly problem for manufacturers that can cause both production issues and lower quality products. This issue can only get worse as winter sets in and temperatures plummet, warns SMC.
The latest digital flow switch to join the SMC family, PF3A7#H, monitors the consumption of the main line with a 100:1 ratio.
SMC has launched an air slide table that is believed to be the most precise, compact and lightweight, offering outstanding performance.
SMC, the worldwide leading expert in pneumatics, has launched a compact cylinder with an integrated linear guide. The innovative MXZ Series benefits from using the design of a compact cylinder, coupled with a linear guide that delivers market leading accuracy and linearity.
COMPAMED 2017 13 -16 November 2017 Düsseldorf Trade Fair, Düsseldorf, Germany Hall 8B, Stand H04 Visitors to this year’s COMPAMED will have a chance to view SMC’s diverse range of specialist solutions for the Life Sciences industry.
SMC has launched a new stainless steel main line filter with 1 µm nominal filtration rating. The AFF#D Series can remove water droplets without the need for an additional water separator, creating greater efficiencies and space savings.
SMC, the worldwide leading expert in pneumatics, has updated its AV directional control valve that consumes as little as 0.35W and is suitable for continuous energising.
SMC has introduced the PSE300AC Series to the monitor market. It simplifies the remote monitoring of different types of sensors being used on a factory floor. Thanks to the display colours and screen layout, the PSE300AC allows three different items to be watched at the same time, enabling operators to view the status of applications at a glance.
The latest VP#17 Series from SMC completes the portfolio of 3 port pressure relief valves for FRL (Filter Regulator Lubricator) units, where electrically operated valves are required.
EMO 2017 18 - 23 September 2017 Hannover Exhibition Centre Hall 6, Stand H66 SMC, a global leader in pneumatic and electrical automation technology, will be taking a step into the future as it reveals its tool box of solutions for operators working towards Industry 4.0 at this year’s EMO.
SMC has launched two air saving speed controllers that reduce energy consumption and are as simple to operate as standard models.
The sharp growth in manufacturing automation and the adoption of the Industrial Internet of Things has seen a rise in interest for SMC’s serial interface solutions.
VXB Series, angle seat valve for air, steam and heated water that delivers an extended operating life, low leakage levels and a compact design, now providing an easy visual check too.
LASER WORLD OF PHOTONICS 2017 26 to 29 June 2017 Munich Trade Fair Centre, Messe, Germany Hall B3, Stand 351 SMC will be revealing its diverse range of cooling and temperature controlling devices that combine both high and constant cooling capacity with optimum cost effectiveness at this year’s Laser World.
SMC, the worldwide leading expert in pneumatics, has recorded another year of growth across its global network, reporting total operating income of €1,187.81 million and net sales of €4,140.72 million [€633.9 million for Europe], an uplift of 3%.
Industry is being offered ‘peace of mind’ in 2017 as SMC highlights the opportunity to improve production and ultimately costs through a focus on efficient temperature control.
As SMC commits to work in partnership with its customers worldwide to drive productivity, performance and energy efficiency, the global automation expert has developed a full range of solutions that have the flexibility to adapt and evolve with its customers’ packaging needs.
In our 24/7 economy and as Governments and industries battle with our thirst for ever increasing supplies of energy, the global automation specialist, SMC, commits to work in partnership with its customers to drive energy efficiency and reduce wastage.
drinktec 2017 11 - 15 September 2017 Messe, Munich Hall B3, Stand 510 SMC, a global leader in pneumatic and electrical automation technology, will be serving up a range of flexible solutions dedicated to the beverage industry at this year’s drinktec from stand 510 in Hall B3.
SMC customers can feel the full force of its electric actuator range thanks to ongoing investment in its product portfolio that now delivers total movement and control for any application.
SMC’s latest compact cylinders, the JMGP guide cylinder and the compact JCQ Series, have been designed with weight and space savings in mind. Both help to reduce machine sizes and costs, and deliver increased efficiency due to their lightweight nature which could enhance cycle time.
SMC’s new 2/3 Port media separated LVMK20/200 valve series has been designed to prevent armature sticking and corrosion that in the past has led to equipment or valve failure. By preventing fluid from entering the solenoid assembly, it remains pollution free from oil, metal and dust particles, improving overall performance and reliability.
INTERPACK 2017 4 to 10 May 2017 Messe, Düsseldorf, Germany Hall 15, Stand D58 Visitors to this year’s INTERPACK will have a chance to view SMC’s energy efficient automation solutions, machine safety components that meet ISO 13849, as well as clean design products for the food industry.
Two new in-line speed controllers from SMC have been unveiled which are quick and easy to set-up and operate. The in-line type AS features a new push-lock knob, offering simple locking and setting. The AS-FS comes with an indicator that allows for accurate adjustments.
TIRE TECHNOLOGY EXPO 2017 14 - 16 February 2017 Hanover Hall 2, Stand 5088 SMC, a global leader in pneumatic and electrical automation technology, will be showcasing its range of products for the Tire industry, focusing on energy efficiency, machine safety and Industry 4.0, at this year’s Tire Technology Expo.