Product selection
×

Go to details
Part number

My account

×

April 2026

SMC received “net-zero target” certification from SBT initiative

SMC is pleased to announce that we have received certification from the Science Based Targets (SBT) initiative*¹, an international certification body for climate change, for our “net-zero target” to reduce greenhouse gas (GHG) emissions across our entire value chain, including Scopes 1, 2, and 3*².

Læs mere
Oplev SMC's robotløsninger live på DIRA Business 2026

Når DIRA Business 2026 løber af stablen, er SMC naturligvis med.

Læs mere

Marts 2026

SMC has been selected for the “A List,” the highest rating in both “Climate Change” and “Water Security” of CDP 2025

SMC is pleased to announce that we have been selected for the “A List” Company— the highest rating by CDP (Carbon Disclosure Project), an international nonprofit organization that evaluates corporate initiatives on environmental issues, in both the “Climate Change” and “Water Security” categories. On March 17, 2026, Ms. Nozomi Tomobe, Executive Officer of SMC attended the “CDP Awards Japan 2026” held at the United Nations University in Tokyo and delivered a speech.

Læs mere
SMC earns energy conservation award, leading by example in energy efficiency and CO₂ reduction

SMC’s energy-saving initiatives at our factories, aiming to reduce greenhouse gas (GHG) emissions; “Challenging the Limits of Air Reduction: Decarbonization through Air-Saving Equipment × Lowering Facility Air Pressure,” won “The Energy Conservation Center, Japan (ECCJ) Chairman’s Award” in the Best Practice Category of the FY2025 Energy Conservation Grand Prize.

Læs mere
SMC strengthens its global innovation capabilities with the launch of the new Japan Technical Center near Tokyo

The new flagship R&D hub will accelerate the development of advanced technologies that directly support SMC’s innovation strategy and customer needs across Europe.

Læs mere

Februar 2026

Simple remote flow setting with new electric speed controller from SMC

SMC launch PFES, an electric speed controller, offering remote control of pneumatic actuator speed with a simple and compact design. It is ideal for installations where access is restricted or puts operators at risk, and it is time saving for applications with multiple speed controllers since the commissioning can be done simultaneously. In case of power loss, PFES retains its last set position ensuring the pneumatic function. Besides pneumatic actuator speed adjustment, PFES is also suitable for the control of air blow or gas purge flow rates.

Læs mere
Washdown-ready bar ionizer by SMC

SMC launches IP66 bar‑type ionizer for washdown and dusty environments Global automation specialist SMC has expanded its static control portfolio with the launch of the IZSW10 Series, a new IP66‑rated bar‑type ionizer designed for reliable performance in dusty, humid and washdown‑intensive environments. The IZSW10 combines high‑speed static neutralisation with long‑range capability, selectable ion generation modes and a hygienic, easy‑to‑maintain design.

Læs mere

Januar 2026

Future proof cooling with SMC’s new CO2 chiller

SMC launches the HR□C series – a compact and energy-efficient chiller range using CO₂ (R744) as a natural refrigerant. Fully compliant with the latest EU F-Gas Regulation (EU 2024/573), this solution is ideal for manufacturers seeking sustainable thermal control without compromising performance or safety. The HR□C series is designed for easy integration into industrial systems and supports a wide range of applications where precise temperature control is critical.

Læs mere

December 2025

New SMC remote control valve brings smart speed adjustment to pneumatic actuators

New from SMC is the PFES Series electric speed controller, offering remote control of pneumatic actuator speed with a simple and compact design. Ideal for installations where access is restricted or puts operators at risk, the PFES Series enables safe, efficient adjustment of actuator speed without the need for manual intervention. Of course, the PFES is not limited to pneumatic actuator speed adjustment and can also be considered for the control of air blow or gas purge flow rates.

Læs mere
Forbedr din maskinsikkerhed med SMC’s nye sikkerhedsafluftningsventil til applikationer med højt flow

For optimal funktionalitet: • Dual-channel ventilkoncept –én enkelt fejl kompromitterer ikke sikkerheden • Certificeret i henhold til ISO 13849-1, op til PLe og SIL 3 i henhold til IEC 61508:2010 – kan installeres som en sikkerhedsrelateret del af styresystemet i overensstemmelse med ovenstående standarder • Høj flowkapacitet – op til 15.000 l/min (ANR) sikrer hurtig afluftning af den farlige energi, som systemtrykket kan udgøre • Soft-start funktion som standard – forhindrer ukontrollerede pneumatiske bevægelser under opstart og reducerer risikoen for maskinskader • Udstyret med port til trykmåler – muliggør visualisering af udgangstryk og/eller integration af yderligere diagnostik med digitale pressostater VPX er modulopbygget for at sikre nem montering sammen med SMC’s luftbehandlingsudstyr og tilsluttes via to M12-stik. Et integreret LED-display giver visuel feedback på ventilens driftsstatus, ud over verifikation gennem styresystemet. “Denne sikkerhedsventil er et velkomment supplement, da den både komplementerer og opgraderer vores sortiment af sikkerhedsprodukter,” siger Fredrik Edholm, Product Manager. “Maskinsikkerhed står øverst på SMC’s dagsorden, og vi leverer effektive produkter til vores kunder, vi bidrager med ekspertise på området, og vi engagerer os i sikkerhedsdrøftelser med vores kunder, hvilket er ekstremt vigtigt,” afslutter han.

Læs mere