Izbira izdelka
×

Košarica (podrobnosti)
Številka artikla

Moj račun

×

Dobrodošli v SMC

Pivovarska industrija

Popolno postrežene rešitve za pivovarne

Postopek varjenja je precej zapleten in za proizvodnjo dobrega piva je potrebno več kot le tehnike varjenja. Enako pomembne so izkušnje iz industrije in poglobljeno poznavanje struktur in procesov v pivovarni.

SMC se zaveda zahtev te industrije, zato se lahko zanesete na našo ekipo usposobljenih strokovnjakov. Pomagamo vam lahko z rešitvami in izboljšavami za vsa področja procesa varjenja in pakiranja. Na primer podaljšanje časa delovanja z izdelki, ki ustrezajo namenu, optimizacija porabe energije, zmanjšanje emisij CO2 in znižanje obratovalnih stroškov.

Storage, process and mixing

With an appropriate monitoring solution, all the variables such as fluid and air pressure and flow rate, tank temperature control, valve positioning and leaks can be under control at any time, making it possible to detect any anomaly beforehand and fix the problems prior to any failure.

Storage, process and mixing

Highlighted Products

Filling

It is essential to monitor the fluid pressure and flow. This way, it’s possible to avoid pressure drops from the air filter, as well as controlling changes due to leaks or a process out of limits. The control of these parameters has a direct impact on the final quality of the product and overall machine efficiency.

Filling

Highlighted Products

Pasteuriser

To guarantee the product meets the appropriate food safety standards, process parameters such as fluid flow, pressure and temperature must be under control. Process limits, leaks, and changes at critical points of the process must be targeted and monitored with suitable equipment.

Pasteuriser

Highlighted Products

Labelling

For consistent labelling, it is necessary to consider air pressure and flow, as well as the maintenance of any ioniser nozzles. If we have these parameters under control, we can monitor for labelling problems at an early stage before any errors occur.

Labelling

Highlighted Products

Case packing and conveying

By monitoring air pressure and flow to avoid restriction and leaks, or checking the nozzles of the static ionizer, you can continue without unplanned stoppages and increase uptime

Case packing and conveying

Highlighted Products

De-palletising and palletising

With the correct monitoring of the parameters, we can detect errors such as loss of vacuum due to pad wear and blocked filters, pressure drops derived from filter air starvation, variations in air consumption due to leaks, and actuator position errors.

De-palletising and palletising

Highlighted Products

“ Splošna učinkovitost opreme (OEE) in vzdrževanje na podlagi stanja (CBM) sta ključni metodi prihranka stroškov za pivovarstvo. SMC v podporo našim strankam ponuja posebne, z IO-Link združljive, komponente in storitve, ki so usklajene z industrijo 4.0. "

Gary Brown | Global Key Account Manager Brewery

Informacije povezane s pivovarsko industrijo

Odkrijte našo paleto izdelkov za potrebe pivovarske industrije

Proces in varjenje

Polnjenje in izpiranje

Kodiranje in označevanje

Transport in pakiranje

Embaliranje in paletiranje

Raziščite SMC Expertise Hub

 

Meeting food industry challenges means having automation specialists directly on the factory floor

 By Diego Mirabelli – Industry Manager Food, Europe 

JUNE 2021
Between 2020 and 2027, the food processing market is expected to grow with a compound annual growth rate (CAGR) of 6.04% according to Verified Market Search. The industry will have to increase its productivity while simultaneously dealing with a lack of workers and cost pressure. 
As most automation companies are focused on machine builders, SMC is differentiating itself by being present with the food manufacturers on their factory floor in order to identify the food industry’s most pressing challenges and help to overcome them.  In order to improve their productivity, factories must reduce downtime, implement more automation and improve energy efficiency, machine safety and hygiene. 

Preberite več