Izbira izdelka
×

Košarica (podrobnosti)
Številka artikla

Moj račun

×

Dobrodošli v SMC

Don’t let actuator maintenance slide

Depending on the series, here at SMC we rate the lifetime of our electric actuators at 5000 km or 30 million cycles without service or maintenance. There are many reasons for this performance level, including robust engineering and testing, alongside internal lubrication that is sufficient for the whole life of the actuator. However, implementing a simple yet considered maintenance schedule supports even more protection for your investment

  By Gerald Rammel, Product Manager Electrical Technology, SMC Austria

APRIL 2023
Depending on the series, here at SMC we rate the lifetime of our electric actuators at 5000 km or 30 million cycles without service or maintenance. There are many reasons for this performance level, including robust engineering and testing, alongside internal lubrication that is sufficient for the whole life of the actuator. However, implementing a simple yet considered maintenance schedule supports even more protection for your investment.

There is no reason to doubt the longevity of your electric actuator. Tests at our headquarters in Japan showed that SMC electric actuators can reach more than twice the aforementioned official lifetime rating without maintenance. But why stop there? Sure enough, maintenance carries a cost, but this is small in comparison with investing in a replacement.

Maintenance intervals
So, how often should you maintain your electric actuator? In reality, the determination of maintenance intervals depends heavily on application-specific operating conditions such as workload, speed, overhang and contamination. For the optimal lifetime of SMC electric actuators, we recommend maintenance activities every 6 months, 1000 km or 5 million cycles, whichever occurs first.

SMC´s Electric Actuator, High Rigidity and High Precision Slider Type – LEKFS Series

Maintenance need not be onerous; simple checks often suffice, such as visually inspecting for loose screws and loose cable connections, along with checking for any increase in vibration or noise. Further maintenance tips include checking the lubricant condition on moving parts, assessing mechanical play in fixed components, and looking for any wear or cuts on the belt.

The belt is a key component, so checking tension is also advisable. A belt that becomes loose could skip a tooth on the pulley, causing positional deviations or allowing the actuator slider to crash into the end of its stroke.

If you don’t feel confident in maintaining your electric actuator, SMC is happy to provide this service.

Selection matters
Another important part of the operating life equation is correct actuator selection. If you are not familiar with selecting electric actuators, why not use our online selection tool? Simply enter details such as the workload and speed to receive a recommendation. Alternatively, please speak directly with our experts. We are always happy to support you in choosing the right product, which in turn helps you to save money and avoid the inconvenience of installing a product that fails due to incorrect selection.

Once specified, we’re also on hand with support on setting up your electric actuator; finding the right parameters and avoiding unwanted effects such as vibration. This so-called ‘tuning’ process also has an influence on operating life. By way of example, exposing the electric motor to vibration could damage internal components like bearings.

Ultimately, electric actuators are robustly engineered products capable of delivering long service life. Nevertheless, options exist to extend this life even further, so why not provide even better protection for your investment?

Discover how with SMC´s Industrial maintenance solutions you will “Keep going”

By Gerald Rammel | Product Manager Electrical Technology, SMC Austria

Gerald first experience in SMC Austria started back in 2011 at local production where he got a good insight of SMC´s products. In 2012, while starting his applied science degree he joined the technical engineering office. This self-defined enthusiastic about technical stuff is at present in the  Electrical Technology team taking care of Product marketing and Know-How of Electric actuators and Fieldbus products.
Gerald dedicates his free time to play music and meet some friends. Although this free time gets limited with the two children he is very happy to see them grow.

Želite biti na tekočem?

Prijavite se na naše mesečne novice in prejemajte tovrstno in drugo vsebino neposredno v svoj nabiralnik.

 

Sledite nam

 

 

Prenesi

 

Morda vas zanima tudi

 

Minimise maintenance by extending the lifetime of your automation components
By Mario Sánchez, Product Specialist Sales Team Manager, SMC Spain
Preberite več 

Counting the real cost of incorrect or poor maintenance
By Julien Caron, Technical Support Manager & Energy Efficiency Leader, SMC France
Preberite več 

IO-Link to move easily to smart sensors
By Mile Milovanovic, Senior Engineer, SMC German Technical Centre
Preberite več 

Making sense of sensors
By Danilo Giordana, Energy Efficiency Project Manager, SMC Italy
Preberite več 

Naj vas navdihne

Preberite o tem, kako stranke oživijo naše izdelke