Izbira izdelka
×

Košarica (podrobnosti)
Številka artikla

Moj račun

×

Dobrodošli v SMC

Sustainable becomes attainable with SMC

The ethos of corporate responsibility, sometimes called corporate social responsibility (CSR) or business sustainability, begins with recognising that the activities of your business impact on society, the environment and the economy, as well as your employees. It makes good sense for your company to operate sustainably as the benefits extend from enhanced brand reputation through to better staff engagement. For sustainability managers at engineering companies, SMC drives sustainable development and delivers a highly positive impact through various CO2 emissions reduction initiatives. These efforts provide a major contribution towards attaining the ISO 14001 environmental management standard, and help any companies reporting their carbon reduction journey based on Scope 1, 2 and 3 emissions, as set out in the GHG (Greenhouse Gas) Protocol.

  By Iván Martínez, Industries Manager, SMC Spain

JANUARY 2023
Here at SMC – an ISO 14001 accredited company since 1999 – we take our CSR seriously in order to promote and support sustainability and, in turn, minimise any negative environmental impact. We’re always looking to develop greener solutions offering CO2 reductions and energy savings that contribute to lower Scope 1, 2 and 3 emissions. To provide a little explanation, Scope 1 covers the emissions that you make directly from running your machines and plant systems, for example. Scope 2 encompasses the emissions that you make indirectly, such as when the electricity you buy for running your machines and systems is being produced on your behalf. Scope 3 covers emissions from the organisations for which your company is responsible, up and down the supply chain. For example, from buying products from your suppliers, and from your products when your customers use them.

Some companies struggle to reduce Scope 1, 2 and 3 emissions. Initially, the improvements are easy, perhaps driven by a switch to green energy. As the CO2 reduction programme advances, however, it becomes harder and harder to identify improvement initiatives. For this reason, our main pillar of sustainability at SMC is continuous improvement. This carefully structured pillar comprises three key areas: sustainable products, air-saving systems and sustainable manufacturing.

Sustainable products – Scope 1
Through assessments, we evaluate the environmental impact of our products in terms of resource savings (smaller, lighter), product longevity, energy savings, amount of packaging materials and waste disposal in order to develop products that support sustainability.

Creating sustainable products relies on factors such as topology optimisation¬, where our innovative design process realises more compact, lightweight products compared with existing solutions. The result: a large reduction in the amount of CO2 emissions created during production.

In addition, our sustainable products contribute to energy savings and less CO2 emissions during their lifecycle, achieving reductions of up to 75%.

Put simply, by using compact, lightweight products, SMC is helping customers to minimise the size and weight of devices and reduce their Scope 1 emissions. We offer sustainable air cylinders, solenoid valves, air filters and one-touch fittings. Further sustainable product innovations that contribute to lower Scope 1 emissions include chillers, which reduce energy consumption by up to 34%. Chillers are an efficient alternative to processes that traditionally employ boilers or furnaces operated by natural gas. In such applications, which include chocolate dosing or paint fluidisation for example, chillers achieve better temperature control but with the great advantage of full electrical operation to help minimise CO2 emissions.

Air-saving systems – Scope 2
SMC can help you to reduce energy consumption and cut your Scope 2 emissions, where the first step of this process is understanding the existing CO2 emissions from your factory. Relatively few are aware that air equipment accounts for about 20% of all factory power consumption. Air blow is the main culprit, responsible for over 40% of all air consumption, with actuators responsible for 14% and vacuum 9%.

Improved air blow efficiency is achievable by selecting optimally sized piping. Similarly, we can help you to save air through device optimisation. SMC has a myriad of devices available that help to reduce air consumption in comparison with conventional alternatives, including impact blow guns (87% reduction), pulse blow valves (50%), vacuum units (93%), digital gap checkers (60%) and booster regulators (40%).

Another initiative is lowering factory operating pressure to 4 bar (from conventional 6 or 7 bar), thus reducing energy consumption by up to 28% without compromising pneumatic performance.

By allowing SMC to check on the status of your factory, we can provide equipment and facility improvement proposals, factory management training and access to a wide range of other useful services that help to lower your Scope 2 emissions.

Sustainable manufacturing – Scope 3
SMC Corporation first achieved accreditation to ISO 14001 way back in December 1999, since when we’ve been promoting a programme of continuous improvement centred on environmental and energy-saving measures at our factories, including the use of solar panels.

Within our many business activities that help to drive down Scope 3 emissions, we target CO2 emissions, water usage, waste discharge and chemical substances usage. Our energy-saving efforts in this area include the use of mechanisms that automatically shut off air sources during plant downtime, which has reduced the use of purge air by around 30%. We also utilise our own flow switches to monitor air flow rates within each factory to allow for early leak detection.

As a point of note, we keep track of any environmental burdens generated through the consumption of resources during the design, development and manufacturing of our products. By resources we mean materials, energy, chemical substances, water, packaging materials and paper.

Support for CO2 reduction
As well as contributing to lower Scope 1, 2 and 3 emissions as part of the GHG Protocol, our sustainable products and initiatives are already helping companies achieve ISO 14001. This standard has a much wider breadth that considers the entire environmental impact, such as waste streams like plastics, metals and oils. Here, SMC has several examples where our products are producing customer benefits, such as wireless fieldbus technology that avoids wiring waste and optimised cylinder design that avoids aluminium waste. ISO 14001 also focuses on recovering energy from waste. Again, we have specific products for this application, where customers reuse spent compressed air before it becomes definitively wasted.

In short, SMC can provide a full range of support options for your CO2 reduction programme, regardless of the methodology you chose to employ or the scale of the challenge ahead.

Discover how to "Energise your efficiency" with SMC

Iván Martínez | Industries Manager, SMC Spain

It was back in 2001, when Iván was still finishing his degree in Engineering that he joined the SMC Spain family. Over 20 years devoted to technical support and sales within the several market industries. Being the first ones the automotive and food sectors and nowadays more focussed on the new emerging markets, such us electric vehicle battery production process; always caring for energy efficiency and for providing key customers with the most innovative solutions available on the market.  
When his 2 teenage kids allow, Iván enjoys photography, indoor climbing and one of most traditional leisure activities: having a beer with his love ones.

Želite biti na tekočem?

Prijavite se na naše mesečne novice in prejemajte tovrstno in drugo vsebino neposredno v svoj nabiralnik.

 

Sledite nam

 

 

Grafični prikaz

Grafični prikaz

Prenesi

 

Morda vas zanima tudi

 

 Fast-track your route to lower energy bills
 By Jeff Careless, Business Development Manager – Continuous Improvement, SMC UK
Preberite več 

SMC can help OEMs develop energy-efficient machines
By Roy Schep, Manager Energy Efficiency, SMC Netherlands
Preberite več 

Energy efficiency: amplifying the benefits of working at 4 bar
By Marek Strojil, Customised services, SMC Czech Republic
Preberite več 

Pneumatic cylinders: drive energy efficiency by switching to 4 bar operating pressure
By Séamus Dunne, Actuator Section Technical Manager, SMC European Technical Centre
Preberite več 

Release the pressure
By Andy Still, Industry Projects Manager, Energy, Europe
Preberite več 

Naj vas navdihne

Preberite o tem, kako stranke oživijo naše izdelke