Saiba mais
Tudo sobre:
Do you need help with the selection?
Soluções industriais
Ecossistema Digital SMC
Indústrias
Documentação
Guias de selecção
Ferramentas de suporte
Novidades
Cultura da empresa
Sobre SMC
SMC Customer cases
Master Production, a niche but highly progressive machine building company from Slovenia, is tapping into the solutions and expertise of SMC to help it drive even more energy efficiencies for customers in sectors such as food and pharmaceutical. With the assistance of SMC, modifications to a cartoning machine for a nutricosmetics manufacturer support use at lower operating pressure, reducing running costs by an impressive 27% a year. As part of a total solution spanning primary, secondary and tertiary packaging processes, Master Production also turned to SMC for a new nitrogen blow solution where the adoption of flow regulation technology is minimising costs.
Read more
SMC components are in the NEREUS system that equips the Cycle building, a Zero-Waste demonstration building. It recycles and reuses in situ all the effluents in the athletes' village.
The SMC products used in Colorservice's automatic plants are key components in ensuring reliability in continuous plant automation and perfect dosing of the raw materials used in the manufacture of tyres from all the world's leading manufacturers. In order to guarantee the highest level of tyre safety and performance, the numerous raw materials that make up tyres must be dosed to perfection. Modern tyres can require dozens of raw materials and additives for their manufacture, which must be carefully mixed and dosed according to the specific recipe required.
In search of an innovative solution, IPTE, the Belgian multinational based in Reus, shared with its technological partner, SMC, the challenge of being able to cool parts during tests in a revolutionary system intended for one of its prestigious Tier 1 electric vehicle clients. The result: a robust, reliable, highly efficient solution, adaptable to various sectors and countries. The key to success has been continuous collaboration, customisation and after-sales service.
Perfectly matched pneumatic and electric solutions for machines that inspect sintered parts and other workpieces. Medical implants, indexable inserts, drills, end mills, gears – the variety of metallic and ceramic components used in different industries is virtually endless. If large quantities are required, many of these components can be produced using sintering. They are often first pressed from powder in a sintering process and then heated. Some of the finished workpieces have to be inspected, labelled and packaged. This is best done automatically, non-stop. To ensure efficient quality assurance, Roboworker has developed RoboInspect, a machine for micrometre-accurate, all-round inspection of workpieces with high requirements. Both there and in other systems of the Roboworker product range, a wide range of electrical and pneumatic automation components from SMC are used.
As part of a commitment to drive a 45% reduction in carbon footprint across its entire value chain by 2030 (and move towards carbon neutrality by 2050), global automotive supplier Valeo is taking advantage of the innovative air-saving initiatives and technologies available from industrial automation specialist SMC. The project, which began at Valeo in France but is rolling out across the group’s international locations, has delivered air consumption reductions of circa 50% in blowing and vacuum applications. Furthermore, reducing shop pressure (when possible) to 4 bar instead of the conventional 7 bar has provided 28% savings in compressed air without any compromise in efficiency.
IMA Fillshape's revolutionary food pouch forming and filling machines leverage SMC solutions to boost productivity and reliability. The flexible plastic pouches are increasingly popular with consumers around the world due to their excellent ease of use. Convenient and lightweight, they first became popular for baby food packaging, but are now widely used for a variety of other products, such as juices, sports drinks and wellness foods
The class-leading service and breadth of products available from SMC is helping a leading machine builder to maintain and extend its prominent position in a highly competitive global market. HACOS designs, produces and installs high-quality chocolate manufacturing machines that spur the development and growth of every size of chocolatier, from artisans to large industrial producers. The company builds from small to very large machines that cover all chocolate manufacturing processes, necessitating the use of a high-calibre technology partner with a proven track record in industrial control and automation.
Sustainability and reduction of energy consumption have been key values for Girbau for many years. The company has recently launched a new ironing unit that is part of a complete automated line. Close collaboration between Girbau and SMC has made it possible to improve ironing quality and achieve an energy saving of 30%, a reduction of 25% in compressed air consumption and a 25% increase in the useful life of textile coatings.
SMC, the world leader in pneumatic automation, and DMC Automation of Turin, which has created a robotic island equipped with SMC components, including an innovative wireless control transmission system, is a solid and stimulating technological partnership oriented towards the search for cutting-edge solutions.
While large companies are focusing entirely on digitisation, many small and medium-sized businesses are dependent on person-to-person support. Instead of investing energy in developing digital platforms, the innovativeness in this segment primarily arises from integrating external expertise into the development process. And this happens in an entirely hands-on, face-to-face manner, rather than virtually. The great success of this method indicates that it won't be going out of style in a hurry.
Sign up to our monthly newsletter and get this type of content, and more, straight to your mailbox
Follow us on Linkedin to discover specialised technical content and keep up-to-date with our events.
Follow us on Youtube to discover the applications of our products.
A more in-depth view on the following topics:
Energy efficiency Air treatment Industry 4.0 Robotics Wireless Fieldbus System
SMC Expertise in: Meeting your challenges
Read on about our Experts’ views on topics, industries, market trends, etc.