Productos seleccionados
×

Ir para detalhes
Referência

Minha conta

×

The SMC Expertise Hub

SMC Expertise in: Meeting your challenges

Because it’s not just about cylinders, valves or even flow sensors. What really matters to us is what you can do with them.

Get some inspiration from when our customers bring our products to life
 

Environmentally friendly water filtration in the athletes' village

SMC components are in the NEREUS system that equips the Cycle building, a Zero-Waste demonstration building. It recycles and reuses in situ all the effluents in the athletes' village.

Read more 

Perfect dosing for perfect tyres

The SMC products used in Colorservice's automatic plants are key components in ensuring reliability in continuous plant automation and perfect dosing of the raw materials used in the manufacture of tyres from all the world's leading manufacturers. In order to guarantee the highest level of tyre safety and performance, the numerous raw materials that make up tyres must be dosed to perfection. Modern tyres can require dozens of raw materials and additives for their manufacture, which must be carefully mixed and dosed according to the specific recipe required.

Read more 

IPTE and SMC are collaborating on the development of an innovative testing solution for temperature control in the manufacture of electric vehicles.

In search of an innovative solution, IPTE, the Belgian multinational based in Reus, shared with its technological partner, SMC, the challenge of being able to cool parts during tests in a revolutionary system intended for one of its prestigious Tier 1 electric vehicle clients. The result: a robust, reliable, highly efficient solution, adaptable to various sectors and countries. The key to success has been continuous collaboration, customisation and after-sales service.

Read more 

Eagle eyes with a soft touch: Full automation versatility for RoboInspect from Roboworker

Perfectly matched pneumatic and electric solutions for machines that inspect sintered parts and other workpieces. Medical implants, indexable inserts, drills, end mills, gears – the variety of metallic and ceramic components used in different industries is virtually endless. If large quantities are required, many of these components can be produced using sintering. They are often first pressed from powder in a sintering process and then heated. Some of the finished workpieces have to be inspected, labelled and packaged. This is best done automatically, non-stop. To ensure efficient quality assurance, Roboworker has developed RoboInspect, a machine for micrometre-accurate, all-round inspection of workpieces with high requirements. Both there and in other systems of the Roboworker product range, a wide range of electrical and pneumatic automation components from SMC are used.

Read more 

SMC drives compressed air efficiency at global automotive supplier Valeo

 

As part of a commitment to drive a 45% reduction in carbon footprint across its entire value chain by 2030 (and move towards carbon neutrality by 2050), global automotive supplier Valeo is taking advantage of the innovative air-saving initiatives and technologies available from industrial automation specialist SMC. The project, which began at Valeo in France but is rolling out across the group’s international locations, has delivered air consumption reductions of circa 50% in blowing and vacuum applications. Furthermore, reducing shop pressure (when possible) to 4 bar instead of the conventional 7 bar has provided 28% savings in compressed air without any compromise in efficiency.

Read more 

Food in pouches: an appealing convenience

IMA Fillshape's revolutionary food pouch forming and filling machines leverage SMC solutions to boost productivity and reliability.
The flexible plastic pouches are increasingly popular with consumers around the world due to their excellent ease of use. Convenient and lightweight, they first became popular for baby food packaging, but are now widely used for a variety of other products, such as juices, sports drinks and wellness foods

Read more 

SMC hits the sweet spot at chocolate machinery manufacturer

The class-leading service and breadth of products available from SMC is helping a leading machine builder to maintain and extend its prominent position in a highly competitive global market. HACOS designs, produces and installs high-quality chocolate manufacturing machines that spur the development and growth of every size of chocolatier, from artisans to large industrial producers. The company builds from small to very large machines that cover all chocolate manufacturing processes, necessitating the use of a high-calibre technology partner with a proven track record in industrial control and automation. 

Read more  

Girbau optimises the energy efficiency of its automated ironing line in collaboration with SMC

Sustainability and reduction of energy consumption have been key values for Girbau for many years. The company has recently launched a new ironing unit that is part of a complete automated line. Close collaboration between Girbau and SMC has made it possible to improve ironing quality and achieve an energy saving of 30%, a reduction of 25% in compressed air consumption and a 25% increase in the useful life of textile coatings.

Read more 

A rebirth in the name of innovation

SMC, the world leader in pneumatic automation, and DMC Automation of Turin, which has created a robotic island equipped with SMC components, including an innovative wireless control transmission system, is a solid and stimulating technological partnership oriented towards the search for cutting-edge solutions.

Read more 

Face to face, not virtual

While large companies are focusing entirely on digitisation, many small and medium-sized businesses are dependent on person-to-person support. Instead of investing energy in developing digital platforms, the innovativeness in this segment primarily arises from integrating external expertise into the development process. And this happens in an entirely hands-on, face-to-face manner, rather than virtually. The great success of this method indicates that it won't be going out of style in a hurry.

Read more 

Want to be up-to-date?

Sign up to our monthly newsletter and get this type of content, and more, straight to your mailbox

 

Follow us

Follow us on Linkedin to discover specialised technical content and keep up-to-date with our events.

Follow us on Youtube to discover the applications of our products.

 

Check out the SMC Experts’ Reports

A more in-depth view on the following topics:

Energy efficiency 

Air treatment 

Industry 4.0 

Robotics 

Wireless Fieldbus System  

 

You may be as well interested in

SMC Expertise in: Meeting your challenges

Read on about our Experts’ views on topics, industries, market trends, etc.