Productos seleccionados
×

Ir para detalhes
Referência

Minha conta

×

SMC’s new 3-screen monitor is latest addition to its sensor family

SMC has introduced the PSE300AC Series to the monitor market. It simplifies the remote monitoring of different types of sensors being used on a factory floor. Thanks to the display colours and screen layout, the PSE300AC allows three different items to be watched at the same time, enabling operators to view the status of applications at a glance.

SMC, the worldwide leading expert in pneumatics, is helping customers to monitor their different remote sensor needs, with the launch of its PSE300AC. It displays different measurement units, so operators can place any sensor remotely on the factory floor.

A spokesperson from SMC said: “The PSE300AC is a welcome addition to our sensor and switch range and has been designed to help simplify the monitoring process for our customers. Ease of use and accuracy of information received will give our customers detailed knowledge about the situation, quickly.”

The PSE300AC is extremely versatile and can be coupled with any type of sensor – including SMC’s PSE5# and PF#5 series – used for pressure, flow or electrostatic. The monitor accepts 1-5 VDC or 4-20mA sensor input signals and features two selectable digital switch outputs, NPN or PNP, that give a signal when a key pressure or range is detected.

What makes the PSE300AC so user friendly is its three screen, multi colour display that makes it very easy to check and set – 3-step, simple and detailed – as all you need to do is press a button to switch between them. The setting is straightforward, with clear screen labelling and selectable colours to indicate when the current value is correct or even incorrect.

Featuring an IP65 enclosure, the PSE300AC offers complete protection against dust, oil and water splashes that makes the monitor robust and able to withstand harsh conditions such as machine tooling environments. In addition, the M12 front face connection reduces the amount of wiring, making it easy to install.

1 de set de 2017