Selezione prodotto
×

Vai ai dettagli
Codice articolo

Il mio account

×

Risparmio di denaro con un sistema di aria compressa efficiente

Imagine coming back from your summer holidays to discover that you left your AC running all that time! Ouch, with today’s high energy prices it would be an expensive shock. In an industrial environment it’s akin to your machines running compressed-air based processes that are un-optimised for idle or standby periods, or where there are undetected air leaks (almost all systems have leaks). You might think the machine isn’t using much energy, but the reality is very different.

  By Filip Běhounek, Customised Services at SMC Czech Republic

JUNE 2023
Some level of idle time is of course inevitable when your workers change shifts or the machine is waiting for input material, so reducing the air pressure in these periods represents a quick way to tackle air inefficiency.

60% energy savings
Take my recent experience at a customer’s facility. As in the majority of energy-efficiency conversations we have with our customers, we start with air consumption monitoring. Could we implement energy-efficiency solutions without monitoring? Yes, but you would miss out on vital knowledge, such as the true ROI (return on investment) or environmental impact of our proposed measures.

Monitoring your compressed air usage, identifying compressed air waste and inefficiencies, and making investments in new compressed air equipment are tangible ways to cut your energy bills. In this instance, my customer’s line was running 6,000 hours a year at an estimated cost of €0.035 per m3. Measurements using an ultrasonic flow meter revealed that the line flow rate during idle time was 123 Nl/min (10 % of the average flow during operation). This 10 % of leakage in that sole line represented a cost of €1,500. However, by automatically reducing the line pressure to 2 bar during idle times, that line saved €900 a year, a 60 % cost reduction.

I can reveal that the facilitating technology in this success was our Air Management System. Notably, this decentralised system is compatible with OPC UA for direct data communications connection without the need of a PLC, as data goes directly to the PC where you are gathering the data. If no monitoring system in place, our Air Management System is capable of working solo. You can parametrise through the web server directly on the Air Management System.

SMC´s Air Management System – AMS20/30/40/60 Series

 

Next-level optimisation
Remember: you cannot manage what it is not measured, so implementing solutions that facilitate virtual visualisation and control of parameters (flow, pressure, temperature) with fieldbus or OPC UA data collection represent a positive step towards higher machine efficiency.

Depending on your situation and budget, you either need a quick fix to impact your operating costs, or you need user-friendly air monitoring or potentially a whole energy optimisation plan. Whatever you decide, SMC can provide you with effective support and highly beneficial outcomes

Discover how to "Energise your efficiency" with SMC

Filip Běhounek | Customised Services at SMC Czech Republic

Filip Běhounek è entrato a far parte della famiglia di SMC Repubblica Ceca subito dopo il diploma. Per i primi due anni si è occupato di assistenza tecnica e, grazie alla grande esperienza acquisita, è passato nel team dei servizi personalizzati. Per molto tempo è stato l'orgoglioso membro più giovane di SMC Repubblica Ceca.

Filip ama i viaggi avventurosi con gli amici, l'esercizio fisico attraverso le tattiche militari e guidare la sua amata auto da rally.

Vuoi rimanere aggiornato sulle novità SMC?

Iscriviti alla nostra newsletter per ricevere news, novità sui prodotti, whitepaper e approfondimenti sulle applicazioni e sulle soluzioni SMC.

Download

 

Potresti essere interessato a:

 

AMS: Il consumo intelligente
di Danilo Giordana, Energy Efficiency Project Manager, SMC Italia
Leggi l'articolo 

 La profonda partnership con i clienti porta a soluzioni di automazione ottimali
di Dan Ives, Senior Project Engineer, European Technical Centre
Leggi l'articolo (EN) 

SMC può aiutare gli OEM a sviluppare macchine ad alta efficienza energetica
di Roy Schep, Manager Energy Efficiency, SMC Netherlands
Leggi l'articolo (EN) 

Ottieni un risparmio energetico del 28% con una pressione ottimizzata dell'aria compressa
di Petr Čečák, Customised services, SMC Czech Republic
Leggi l'articolo 

Ridurre la pressione
di Andy Still, Industry Projects Manager, Energy, Europe
Leggi l'articolo 

Scopri come i nostri clienti danno vita ai nostri prodotti