Attuatori
Attuatori elettrici
Valvole per il controllo direzionale
Tubi e Raccordi
Controllo fluidi
Sensori di rilevamento
Controllo della temperatura
Prodotti per camera bianca
Scopri di più
Ricerca per Funzionalità
Sustainability and reduction of energy consumption have been key values for Girbau for many years. The company has recently launched a new ironing unit that is part of a complete automated line. Close collaboration between Girbau and SMC has made it possible to improve ironing quality and achieve an energy saving of 30%, a reduction of 25% in compressed air consumption and a 25% increase in the useful life of textile coatings.
Leggi il customer case
In the vast market for packaging machinery, the Swiss company EmbaPlan GmbH specialises in the development and manufacture of flexible filling machines for small quantity production runs, adapted to the needs of innovative and regional producers of high-quality foods. The company recently made a major upgrade to one of their filling machine models, adding a valve manifold from SMC for extra flexibility and performance.
Is there a draught? If the answer is “yes”, then the window frame or door frame doesn’t fit properly. To ensure your home stays warm and the doors and windows to look attractive, all parts for these products need to be produced with great precision and sanded to perfection. Conventional all-around sanders can only be used either for window or door components. With just a minor design change, MB Maschinenbau has now made its ROBA Fentech profile sanding machine for wooden window profiles also suitable for door frames. When combined with an optical sensor, the D-MP position sensor from SMC ensures that the machine optimally recognizes all workpieces.
Worthmann has developed a helium leak-tightness test system, which uses high vacuum and mass spectrometers to identify even the smallest leaks in components – and it takes only one minute. High-vacuum angle valves from SMC’s XLA series provide the long service life and robustness necessary for the task.
While large companies are focusing entirely on digitisation, many small and medium-sized businesses are dependent on person-to-person support. Instead of investing energy in developing digital platforms, the innovativeness in this segment primarily arises from integrating external expertise into the development process. And this happens in an entirely hands-on, face-to-face manner, rather than virtually. The great success of this method indicates that it won't be going out of style in a hurry.
L'azienda torinese DMC Automation ha realizzato un'isola robotizzata equipaggiata con componentistica SMC, tra cui spicca un innovativo sistema di trasmissione di controlli wireless. Quella tra SMC e DMC Automation è una partnership tecnologica solida e stimolante, orientata alla ricerca di soluzioni all'avanguardia.
L'offerta completa di componenti per l'automazione pneumatica di SMC e la sua presenza globale aitano Fosber - uno dei protagonisti del mercato globale delle linee per la produzione di cartone ondulato - a proporre soluzioni complete estremamente affidabili.
Iscriviti alla nostra newsletter per ricevere news, novità sui prodotti, whitepaper e approfondimenti sulle applicazioni e sulle soluzioni SMC.
Energy Efficiency Trattamento aria Industria 4.0 Robotica e Cobotica
Scopri e leggi gli articoli dei nostri esperti