Cesta de productos
×

Ir a detalles
Referencia

Mi cuenta

×

Dial into remote assistance for your equipment

Although there are many bigger advantages to the adoption of industrial communications, one of the benefits you can tap into very quickly is the enablement of remote assistance. By implementing a system such as the SMC webserver, our remote teams can access your historical data and easily analyse the possible causes of your failure or malfunction. Our webserver offers short ROI for both users and machine builders as they can avoid expensive travel costs and provide an extremely reactive service.

  By Massimo Gazzaniga, Technical Support Engineer Mechatronics & Network Manager, SMC Italy


SEPTEMBER 2022
How does it work?
Reading data via our webserver is extremely easy; you only need a standard PC with a network card. With SMC’s webserver it’s possible to read different types of data, according to whichever device is in use. Our electric actuator controllers and serial interfaces offer webserver compatibility.

What kind of data do you get?
With regard to electric actuator controllers, the most important data sets to read are those for speed and torque. Further notable requirements include the potential to change parameter settings for very fast commissioning in remote applications (via webserver) and relaying common driver alarms, such as overload.

Concerning serial interfaces, the most important data to set are the range of analogue values. As a point of note, it’s possible to integrate the IO-Link master unit with our EX600 fieldbus system platform, a modular solution for reading very different types of sensors and devices. The ability to command your valves without the use of a PLC is also important.

Recreation – SMC´s IO-Link system configuration

 

Multiple benefits
If the right IIoT platform is in place, our devices generate a lot of data that offers a myriad of advantages for users, such as smart maintenance or energy savings. In short, any applications can benefit from our smart devices with industrial protocol communication capabilities.

As a next step, here at SMC Italia we started to use augmented reality (AR) glasses, helping the user to execute maintenance or problem-solving tasks with the help of an SMC expert. As you can see, we constantly strive to provide our customers with easy, cost-effective, added-value solutions that make a genuine difference to business operations through improved efficiencies. It’s time for us to communicate.

Descubra cómo SMC es su socio para la IIoT

By Massimo Gazzaniga | Technical Support Engineer Mechatronics & Network Manager, SMC Italy

“Since I was a child, electricity has been my passion, I was 8 years old and I got the shock trying to repair the light switch in my bedroom and at 12 I tried the first little programs with the commodore 64”.
25 years of work experience inmerse in industrial automation, plc software creation and always captivated by the world made up of wiring, processes, energy, communication protocols. A very useful bagage in this historical period marked by industry 4.0 and smart factory. Massimo faces all those challenges in his amazing work in mechatronics and serial interface devices technical support at SMC Italy.
Massimo´s hobbies are running and swimming and become a child again, playing with his daughter Margherita.

 

¡Síguenos!

Síguenos en Linkedin para descubrir contenido técnico especializado y estar al día de nuestros eventos.

Síguenos en Youtube para descubrir las aplicaciones de nuestros productos.

 

Downloadables

 

También te puede interesar

 

Click to configure Rich text snippet

Click to configure Rich text snippet

SMC Expertise: Comprendemos tus retos diarios

Sigue leyendo para descubrir cómo nuestros clientes dan vida a nuestros productos