Hot on the heels of Lean Manufacturing, the focus has once again changed.
With the goal to improve manufacturing performance, using more automated operations and the use of data analytics, smart manufacturing is the order of the day. This technology-driven approach, using machinery connected to the internet to monitor the production process, has seen the development of smart machine components.
SMC's IO-Link products can help you improve your productivity and reduce your costs, granting dynamic production processes and leading to the Smart Flexibility the industry is seeking. Plus, they will let you bet on the continuous improvement of your company’s industrial maintenance strategy.
For more information on our smart machine solutions check out our latest products on our website today.
IO-Link (IEC61131-9) is an open standard technology that allows the bidirectional data exchange from sensors and devices that support IO-Link and are connected to a master.Thanks to an IO-Link master, data is transmitted over various networks, fieldbuses, or backplane buses, making the data accessible for immediate action or long-term analysis via an industrial information system (PLC, HMI, etc.).
Make profit of the latest technology thanks to the combination of both, wireless and IO-Link communications
Data transparency from the sensors and actuators level all the way to the automation level through an IO-Link unit.
Expect a diverse range for measuring flow, pressure, vacuum, actuator position and condensation allowing the exchange of diagnostic data to the automation level.
Transmission of parameterization data to the actuator through IO-Link
There are three primary data types made available, which are categorised into cyclic data (data automatically transmitted on a regular basis) or acyclic data (data transmitted as needed or upon request).
No need to wait for a process failure to replace a sensor.
With the implementation of the IO-Link technology, the devices are always being monitored to know the state of their health with Event Data.
Depending on the device, you can track if they are suffering excessive temperature, pressure, if they are out of range, internal default, etc.
The entire measured value transmission is digital, thus, all device parameters are stored in the IO-Link unit. The data transfer is based on a 24 V-signal and the shielded wires are not required.
Customised solutions force a continuous change in parameters. The overall setting control from the control system (PC) minimises time, increasing machine availability.
Plug & play replacement simplifies the connection: a common connector for communication and power. Parameters are saved in the master, enabling automatic setting once the device is connected.
The key-lock function keeps unauthorised persons from tampering with the settings.
|
IO-Link to move easily to smart sensors |
Ask our experts today!