This software basically calculates the pressure drop or maximum flow rate for a pipe. Why is it interesting for you to know this information?
When talking about an installation that includes, for example, linear actuators, grippers or even valves, it is fundamental to know the pressure to see if it is possible to activate the components and if it will be possible to achieve the required force with the elements involved. With a very long or over-dimensioned pipe, there may can be a pressure drop that leads to a malfunction in the installation.