Mehr erfahren
Allgemeine Produktinformationen
Online-Seminare
Trainings
Wir freuen uns, Ihnen mitteilen zu können, dass SMC sein derzeitiges Technisches Zentrum in Tsukuba (JTC) verlagert und erweitert. Im Herbst 2025 wird demnach das "Kashiwanoha Campus New Technical Center (vorläufiger Name)" in der "Kashiwanoha Smart City" eröffnen, das den Kern der Forschung und Entwicklung von SMC bilden wird.
SMC Corporation, a global leader in manufacturing comprehensive automation control equipment has been recognized by Forbes magazine as a World’s Best Employers 2022.
SMC is introducing the new EXW1 Series Compact Wireless System with an increased range of up to 100 m. Similar in technology to the current EX600-W, the EXW1 is smaller, lighter and fieldbus compatible, and with improved features that augment the current portfolio.
SMC, a leading Japan-headquartered global specialist in pneumatic and other automated control solutions, is set to join the Nikkei 225 (or Nikkei Stock Average), the premier and most-often quoted index of Japanese stocks. The Nikkei 225 comprises of 225 stocks selected from Japan’s top-performing and most liquid blue-chip companies. SMC will commence its listing on 3 October 2022.
SMC’s ISE7# pressure switch has been updated adding higher pressure ranges apart from offering improved flexibility and higher control of applications, leading to better decision making.
The new JSY & ZK2-A valve and ejector combination manifold from SMC not only simplifies pneumatic systems in applications requiring both positive and negative pressure (vacuum), it also reduces wiring requirements, provides complete compatibility with multiple fieldbus communication protocols and eliminates pressure fluctuations.
Any machine builder looking to simplify and reduce the cost of adding higher levels of safety, while simultaneously seeking faster and broader communication capabilities should consider the new JXCLF step motor controller from SMC. The JXCLF features an IO-Link communication interface and a Safe Torque Off (STO) function, thus presenting machine builders with the opportunity to deliver better control of the manufacturing process and increase their system’s safety integrity level (SIL 3) and performance level (PL e) in a cost-effective way.
Leading industrial control and automation solutions specialist, SMC, is adding a new range of pinch valves to its expansive offer for medical device and food system OEMs. With the new LPV series valve, fluid does not come into contact with any moving parts, avoiding the potential for contamination. Moreover, by simply discarding the tube after use, there is no longer any need for a washing process, ensuring good hygiene. SMC’s energy-saving LPV pinch valve is suitable for controlling a wide range of analytical, medical and food industry fluids.
General industrial equipment designers, manufacturers and maintainers can now benefit from the new SMC ZKJ vacuum manifold with PROFINET-enabled communication for remotely controlling and monitoring manufacturing processes. The ZKJ also offers impressive suction flow rate taking its low air consumption and low power consumption specifications into account. Other features include valve protection functionality, IP65 rating and the ability to control up to 16 ejectors with a single manifold.
The new JSY5000-H valve manifold from SMC is purpose-designed for use in food and beverage manufacturing plants, as well as breweries. Featuring a clean design to cope with regular wash-downs, the IP69K-compliant valve differentiates itself in the marketplace with its high flow rate, low power consumption and IO-Link point-to-point communication capability, bringing a new level of control to production.
One of the latest digital flow switches to join the SMC family, PF3A#H, monitors the consumption of the main line with a 100:1 ratio. It is IO-Link compatible, and it offers the possibility of being connected to air combination units in a simple way. And now, an even more complete solution can be obtained, thanks to the integrated pressure and temperature sensors.
A new polypropylene type pump from SMC has been designed to withstand the harshest manufacturing processes, delivering production reliability that lead to cost and energy savings.
Das Umwelt- und Nachhaltigkeitsbewusstsein von Verbrauchern steigt weltweit, und die Prinzipien der Kreislaufwirtschaft werden auch in der Produktion immer mehr umgesetzt. Die Verpackungsindustrie steht damit vor neuen Aufgaben: Gefragt sind Materialien, die leichter wiederverwendet werden können – wie einschichtiger Kunststoff oder Papier – aber auch eine Reduktion der eingesetzten Materialmengen. Das bringt technische Herausforderungen für Verpackungsmaschinen mit sich. Von Jorge Salgado, Food & Packaging Industry Manager, SMC Spanien
Das Turiner Unternehmen DMC Automation baut eine Roboterinsel, die mit SMC-Komponenten ausgestattet ist, darunter das innovative drahtlose Feldbussystem EX600W. In ihrer langjährigen technologischen Partnerschaft sind beide Unternehmen auf innovative Lösungen fokussiert.
Zwischen 2020 und 2027 wird das Marktvolumen für Lebensmittelverarbeitung laut Verified Market Search voraussichtlich im Durchschnitt um rund 6 % jährlich wachsen. Die Industrie wird demnach ihre Produktivität steigern müssen, ist aber gleichzeitig mit einem Fachkräftemangel und Kostendruck konfrontiert. Von Diego Mirabelli (SMC Industry Manager Food, Europe)
Nachhaltigkeit und Reduzierung des Energieverbrauchs sind für Girbau, Hersteller von Wäschereimaschinen, seit vielen Jahren wichtige Werte. Das Unternehmen hat kürzlich eine neue Bügelstation auf den Markt gebracht, die Teil einer komplett automatisierten Linie ist. Durch die enge Zusammenarbeit zwischen Girbau und SMC konnte die Bügelqualität verbessert und eine Energieeinsparung von 30 %, eine Reduzierung des Druckluftverbrauchs um 25 % und eine Erhöhung der Nutzungsdauer der Textilbeschichtungen um 25 % erreicht werden.
Pneumatische Anlagen machen ca. 20 % des gesamten Stromverbrauchs in Fabriken aus. Aber es gibt Abhilfe, die Energieeffizienz zu verbessern – indem der Betriebsdruck gesenkt wird. Wie dieses Ziel erreicht und dem wichtigsten aktuellen Trend in der Fertigung nachgekommen werden kann, schildert SMC-Experte Andy Still (Industry Projects Manager, Energy).
Ich bin Yoshiki Takada. Per 1. April 2021 wurde ich zum neuen Präsidenten der SMC Corporation ernannt. Seit unserer Gründung im Jahr 1959 hat sich SMC zu einem führenden Hersteller in der industriellen Automation, insbesondere pneumatischer und elektrischer Anlagen, entwickelt. Unser Ziel ist es, stets alle Kundenwünsche zu erfüllen.
The new HRR rack-mounted thermo-chiller from SMC has been designed for installers where space is an issue. It also delivers efficiencies in terms of installation and maintenance, as it can be adjusted and maintained while installed in a rack.
Während die Robotik den Weg für das rasante Wachstum der Automatisierung ebnete, können Cobots als Demokratisierung der Robotik-Technologie verstanden werden. Sie eliminieren Kosten und jene komplexe Programmierung, die Roboter normalerweise erfordern. Gleichzeitig bieten sie ein stark gesteigertes Maß an Flexibilität. Von Andrea Trifone, Cobot Project Leader, SMC Italien
SMC has designed a direct operated 2-port solenoid valve that can withstand the harshest of environments whilst saving energy.
SMC has designed a new lightweight, handysized ionizing gun that can neutralise static, rapidly and effectively, from a variety of products at different phases of production.
Hochvakuum-Eckventile von SMC sorgen für saubere und präzise Dichtheitsprüfungen bei Worthmann
Der Maschinenbau hat das im Rennsport und in der Flugzeugindustrie geltende Prinzip für sich entdeckt: Gewicht sparen und so höhere Geschwindigkeit erzielen. Gerade Roboterarme sind starken Momenten und kinetischen Energien ausgesetzt. Schafft man es, die Gewichte zu reduzieren, lassen sich höhere Geschwindigkeiten fahren – oder man kann den gesamten Roboter kleiner und damit kostengünstiger wählen. Der Hersteller SMC macht es vor.
Im großen Markt des Verpackungsmaschinenbaus konzentriert sich die Schweizer EmbaPlan GmbH auf flexible Abfüllanlagen für kleine Stückzahlen. Damit richtet sich EmbaPlan an innovative und regionale Erzeuger von hochwertigen Lebensmitteln. Das Unternehmen hat kürzlich eine Maschinenbaureihe grundlegend überarbeitet und mit einer Ventilinsel von SMC zusätzliche Flexibilität und Leistung in die Anlagen eingebracht.