Produktvalg
×

Gå til detaljer
Varenummer

My account

×

Making sense of sensors

Such is the evolutionary rate of change in modern manufacturing that failing to keep pace with the industry’s shift to digitalisation – and its associated efficiency and productivity benefits – can prove extremely costly. But where to begin? Most professionals in this space point to data collection as the first step, because subsequent data analysis can support the adoption of predictive maintenance strategies, better decision-making and continuous process improvements. However, it is only possible to fulfil this ambition by adopting the optimal sensor for the application.

  By Danilo Giordana, Energy Efficiency Project Manager, SMC Italy


DECEMBER 2021
Such is the evolutionary rate of change in modern manufacturing that failing to keep pace with the industry’s shift to digitalisation – and its associated efficiency and productivity benefits – can prove extremely costly. But where to begin? Most professionals in this space point to data collection as the first step, because subsequent data analysis can support the adoption of predictive maintenance strategies, better decision-making and continuous process improvements. However, it is only possible to fulfil this ambition by adopting the optimal sensor for the application.

Pneumatic systems are widespread across a wide range of industrial machines, systems and equipment, and represent a common starting point for many digitalisation projects, offering a short return on investment. Here, three electronic sensor types are prevalent: flow, pressure and position.

As well as monitoring the consumption of compressed air, flow sensors can also check for blowing performance in applications such as cleaning, cooling, suction verification, leak test, determination of cooling status/cooling water problems (integrated temperature sensor).

SMC´s 3-Colour Display Modular Digital Flow Switch with Pressure/Temperature Sensor - PF3A8#H Series -
Connectable to FRL air combination units and with integrated temperature and pressure sensor, all in one solution. IO-Link compatible.

 

SMC´s High-Precision Digital Pressure Switch, ZSE/ISE20 Series. This switch, measures air, non-corrosive gas or general fluids. It counts with a screen that displays not only the measured value (current value) but other relevant ones (set value, hysteresis value, bottom value or peak value) at a glance. IO-Link compatible.

 

Position sensors are also important for predictive maintenance project as it will detect failure of the main critical device: the actuators. For example, position sensors can provide information about a reduction in actuator speed. Matching this speed data with flow data, it is possible to provide a quick evaluation if a given actuator needs to be replaced.

Through analysis of the data provided by sensors, machine users are able to define the machine’s ‘zero point’, namely the standard performance benchmark. From here, it becomes simple to deliver two important outcomes: understanding if something is deviating from the typical curve (and thus predicting oncoming faults as part of a targeted maintenance strategy); and identifying potential process improvements.

With the right sensors, manufacturing and process plants can take advantage of both historic and real-time data, with the latter essential to prevent ‘the unpredictable’ before it gets out of hand. After all, a minor fault often leads to a bigger and more expensive one.

SMC offers a wide portfolio of sensors, covering all customer requirements from simple on/off signal solutions to those that support IO-Link. All of the company’s sensors are simple to install and use, allowing customers to set their own parameters in accordance with the key metrics of the machine or application. If there is any doubt, SMC’s team of experts is always ready to provide advice and support.

 

Discover how with SMC´s Industrial maintenance solutions you will “Keep going”

By Danilo Giordana | Energy Efficiency Project Manager, SMC Italy

Danilo har omfattende ekspertise inden for pneumatikfeltet, hvor han har været involveret siden 1986. I år 2000 blev han en del af SMC Italia-familien, først som teknisk supportingeniør og senere i salgsafdelingen, hvor han arbejdede med flere nøgleprojekter. Siden 2020 har han været ansvarlig for energieffektivitetsområdet i Italien.

I sin fritid elsker han at vandre sammen med sin kone og deres hund. Danilo nyder at læse bøger samt at skrive romaner (på nuværende tidspunkt, venter han på den store succes,... desværre er de kun tilgængelige på italiensk...).

Vil du være opdateret?

Tilmeld dig vores månedlige nyhedsbrev og få nyheder og mere indhold som dette direkte i din indbakke

 

Følg os

 

Downloadables

 

Måske er du også interesseret i:

 

Vedligehold: SMC anviser hvorfor 'P' i prædiktiv vedligeholdelse står for progres - og ikke pine
Af Oliver Prang, Expert Digital Business Development, SMC Tyskland
Læs mere 

IO-Link gør det nemt at skifte til smarte sensorer
Af Mile Milovanovic, Senior Engineer, SMC's Tekniske Center i Tyskland
Læs mere 

Get some inspiration from when our customers bring our products to life.