Избор на продукт
×

Подробен изглед
Артикулен номер

Моят профил

×

Fast-track your route to lower energy bills

In an era where manufacturing and process plants are under increasing pressure from soaring energy bills and ever-tightening CO2 emissions legislation, it begs the question: is there a way to reduce my energy consumption quickly without compromising efficiency or output? The short answer is yes, with the right advice and expertise.

  By Jeff Careless, Business Development Manager – Continuous Improvement, SMC UK

JANUARY 2023
Energy and carbon footprint have long-proved a hot topic for users of compressed air as it represents as much as 20% of all factory power consumption. Here, based on our experience, we set out five ways that deliver fast and effective energy reductions.

Relieve the pressure
The first way is to reduce the pressure of your compressed air system where possible. For most industrial plants, typical operating pressure is between 6 and 7 bar. By lowering your pressure to 4 bar, energy consumption reduces by up to 29%. However, expert input is required to avoid compromising performance.

Plug leaks
We’ve encountered plants suffering from 20-50% leakage rates, driving up energy consumption and bills. The optimal way to identify leaks is by appointing an expert company to undertake an audit, ideally twice a year. However, for those seeking a quicker route to improvements, shut-off solenoid valves prevent air losses to leaks even when machines are idle. Other solutions include a two-pressure module which switches to a lower pressure during machine idle periods, vastly reducing leakage, or the new plug and play SMC Air Management System, for example.

SMC´s Air Management System Level up your compressed air management

 

Blowing applications
Did you know that air-blow tasks are accountable for more than 40% of your factory air consumption, thus offering a real savings opportunity? Here, sizing your blow nozzles correctly, coupled with a reduction in factory pressure, delivers good results. Further initiatives in this area include better use of regulators to ensure you only use the amount of air necessary. Pulse-blow valves, which switch the air blow on/off very quickly while maintaining the force of the blow, offer another great way to reduce your air consumption, sometimes up to 50%.

SMC´s Pulse Blow Valve – Save on blowing air

 

Efficient vacuum systems
If you have machinery using air-generated vacuum pick and place applications, the use of vacuum ejectors with multiple Venturi and air switch-off energy-saving technology reduces air consumption by up to 93%.

SMC´s Vacuum Unit – The all-in-one silent energy saving solution

 

Right components
We always say at SMC that energy and cost efficiency is deliverable through many small actions. Choosing components wisely makes a big difference. For example, adding power-saving circuits to your solenoid valves, a speed controller to your cylinders or using triple inverter technology in your thermo-chillers, eases energy bills.

From our experience we know that these five tips reduce energy bills, fast. The only caveat is tapping into the right advice and expertise. So don’t delay: ask our experts to help start your energy-reduction project.

Discover how to "Energise your efficiency" with SMC

Jeff Careless | Business Development Manager – Continuous Improvement, SMC UK

Jeff has over 35 years of experience working in the SMC UK sales team which has seen him assume the roles of Regional Sales Manager and numerous specialist roles on customer energy saving projects. Away from work, Jeff has been an FA accredited football coach for 13 years and you can find him on the touchline coaching local football teams across Birmingham during weekends. In addition, Jeff enjoys spending time in the terraces at Villa Park with his two sons watching his beloved Aston Villa. Cruise holidays with wife Jacky and entertaining their grandchildren make up the rest of his time. 

Искате да сте в крак с времето?

Абонирайте се за нашия ежемесечен бюлетин с новини и ще ще ви държим информирани с електронно писмо директно изпратено до вашата електронна поща

 

Последвайте ни

 

Документи за изтегляне

 

Това също може да ви се стори интересно

 

 Устойчивостта е постижима с SMC
От Iván Martínez, Industries Manager, SMC Spain
Научете повече 

SMC може да помогне на производителите на оригинално оборудване да разработят енергийно ефективни машини
От Roy Schep, Manager Energy Efficiency, SMC Netherlands
Научете повече 

Енергийна ефективност: ползите за вас при работата на 4 бара
От Marek Strojil, Customised services, SMC Czech Republic
Научете повече 

Пневматични цилиндри: повишаване на енергийната ефективност чрез преминаване към работно налягане от 4 бара
От Séamus Dunne, Actuator Section Technical Manager, SMC European Technical Centre
Научете повече 

Освобождаване на налягането
От Andy Still, Industry Projects Manager, Energy, Europe
Научете повече 

Дългогодишен опит в справяне с ежедневните ви предизвикателства

Прочетете как наши клиенти вдъхват живот на компонентите